Hello Prateek
Yes, that is correct. Also when debugging such an issue make sure you have 2 things in place i.e. Stimulus and control
1. The input signal is not defined here as a static value or changing value. Always have a static value so that…
Hello Jame,
It is a general problem with the EVM you are using. While capable of doing low level audio, the EVM isn't going to produce crystal clear sounds without significant help from external chips like audio codecs. The TM4C device is not an audio…
Other Parts Discussed in Thread: UNIFLASH , LMFLASHPROGRAMMER , TM4C1294NCPDT Hi all,
There is a TIDM-TM4C129POEAUDIO (Audio Communication with Power Over Ethernet) project made by Amit Ashara . Please use the link to get more details. The thread has…
Hi,
First of all, your screenshot is really hard to see the detail. In the future, you should attach PDF. From a high level, I don't see a protection diode between the MCU and the RJ45. Without the protection diode the MCU can be damaged only partially…