Part Number: TM4C1237E6PM Other Parts Discussed in Thread: CC1352P Hi community,
In one of our project, we are using TM4C1237E6PM microcontroller to support the USB OTG feature.
During USB host mode, connected device will be powered on via VBUS…
I will need some clarification on your issue. Did you start with a blank TM4C1237E6PM on a custom board? Then you used the ROM based USB DFU bootloader to program your code into the device. After that, you no longer have USB connectivity. Is that correct…
Part Number: TM4C1237E6PM Hi community,
What is the USB classes supported by TM4C1237E6PM microcontroller ?
Is this micro controller supports CDC Class ?
Thanks & regards,
Divya
Part Number: TM4C1237E6PM I have been using LM Flash Programmer for weeks to program the TM4C device on our custom board. I am using the USB DFU configuration. I made yet another change to the code, entered the dfu command in my TeraTerm window, and then…
Hi Utpal,
See below.
utpal kumar said: 1> Pin PBI/USBOVBUS will sustain 5 v input as VDD is 3.3 volt.
Refer to the schematic of the Tiva Launchpad.
utpal kumar said: 2>what is programming procedure ? if I will not go in Hibernation mode , CPU…
Other Parts Discussed in Thread: TM4C1237E6PM Hi,
I am working on a design that uses the Tiva TM4C1237E6PM device. I am running very low on GPIO pins and would like to reclaim unused ADC inputs. I used the pin mux tool to assign my I/O, and when I enable…
Hello Amit,
I've been hunting for any resolution to this problem or example to setting BOR on TM4C1237E6PM.
Please provide an example. What Aman has suggested as an example won't work on the TM4C1237E6PM because there is no 'delay' field in the PBORCTL…