I m using board TMDSEVM6678.I have doubt regarding how to use all the cores for processing.Right now I m using only one core for the program client_evmc6678l.When i try connecting all the cores,CCS is not responding.Can someone please help....
S.No
Part number
Family
Linux SDK
Linux RT SDK
RTOS SDK
CCS version
Other tools
1
66AK2H06
K2H
PROCESSOR-SDK-LINUX-K2HK 06_03_00_106
PROCESSOR-SDK-LINUX-RT-K2HK 06_03_00_106
PROCESSOR-SDK-RTOS-K2HK 06_03_00_106
CCSTUDIO_9…
Hi Yewkui Wang,
please use MCSDK on C6678 and let us know if you come across any questions.
Please download the MCSDK and other related documents for C6678 using the websites below.
As of now, we are closing this thread as answered.
…
Joe,
Are you using external XDS560 emulator ? Have you tried connecting the target using on board emulator ?
Have you created a target configuration and could able to pass the test connection ?
Regarding software, you could see all the relevant…
Hi,
I want to read and write from DDR3 into L2 memory. How can i start the interface, is there any example project ?
I am working on TMDSEVM6678 and CCS version 5.4
Regards,
Vamshi
Hi Senthil,
I am referring to the table on the following page http://www.ti.com/tool/tmdsevm6678 which I am pasting below for ease of reference. I am taking the "Current version" column to mean silicon revision available on the EVM. Is that a correct…
Hi Rajasekaran,
Thank you for the response.
I am using an EVM (TMDSEVM6678).
I am not quite sure I understand your second question? I am purely measuring the outputs on the EVM's SPI pins for now, in order to make sure that they are outputting the…
Hi Pubesh,
the project now runs as expected. The error was in my linker-file. The TMDSEVM6678 got 4GBit DDR3. So 4GBit != 4Gbyte. My mapping for each core was 512MB, so I simple run out of memory.
Thanks for the patience and help
Patrick
Hi Vidya, TMS320C6678 could fit your needs. This is a multicore DSP (8x C66x cores), each core runs at 1.0 to 1.25 GHz enabling a total of 10 GHz per chip. For more details please visit: www.ti.com/.../TMS320C6678
For C6678 device we have a collection…
Hi Vasishth Desai,
Just answering part of your questions (I don't know the other answers). 6678 has the highest processing power of those devices you mentioned, but maybe it's not the more suitable for your application or you don't need all of its processing…