Other Parts Discussed in Thread: SYSBIOS Hi,
I am a new user of board TMDSEVM6678 .I need to develop an ethernet application ,for that I'm depending on client_evmc6678l RTSC project to understand the flow.I have some doubts regarding this matter.
…
Now I am using 2 TMDSEVM6678 boards connected with BOC board. I want to use OpenMP programming on multi dsps through SRIO,how can I do? How to write a .cfg file?
Thank You!
Hi sir,
I have doubt regarding TMDSEVM6678 spi programming.
That is, what boot configuration should I need to maintain to run my own Source code for SPI.
thank you sir.
regards,
chandu.
Hi Kazuhito,
I'm researching your questions further. I wanted to get some more insight into your setup:
Are you having issues running this example?
Are you running on the C6678 EVM ( TMDSEVM6678 )?
Thanks,
Clinton
I have two applications that I would like to boot to different cores on both a TMDSEVM6678 and TMDSEVM6670. Both are developed under CCSv5 and are in elf format. Image A would boot on Core0; Image B would boot on all other cores.
I'm having a hard time…
Hi soon,
Can you share more about your setup?
Are you using the C6678 EVM ( TMDSEVM6678 )?
Are you using the Bridge over Card (BoC) board ( CI2EVMBOC ) to connect your 2 devices?
What are the 2 devices you have connected to each other communicating…
Other Parts Discussed in Thread: SYSBIOS Hi guys,
im new to TI DSP multicore, im using TMDSEVM6678 (and this is my first post :) )
I cannot compile the example mcsdk demo, image processing with openMP
i loaded the demo and the only thing that…
Other Parts Discussed in Thread: SYSBIOS Hi,
I am using TMDSEVM6678 board for running HUA demo with switch settings given in demonstration guide but i am facing the following error. i am attaching the console statements. please help me in solving this…
Hi Kazu,
Yes, sorry I've confused the processors.
For your questions 2, 3 & 4, my comment still applies for TMS320C6654 devices.
Q1: Note 3(blue) is applied to each capacitor in CVDD1, but Note 1(red) is applied to only 560 pF in CVDD. I guess…
Hello Yungao,
1) Yes, this is supported, you can find more details here:
http://linux-c6x.org/wiki/index.php/GDB
2) Yes, however, I would strongly recommend a low cost EVM. E.g.,
TMS320C6678 Lite Evaluation Module only costs $399 http://www.ti…