Part Number: TMDXSK437X Other Parts Discussed in Thread: AM4378 , If the MPU AM4378 is configured as CPSW, and one RJ45 (J6 in the TMDXSK437X EVM) is connected with TCP/IP ethernet, the other RJ45 (J8 in the TMDXSK437X EVM) is connected with Ethercat…
Part Number: TMDXSK437X
Hi
I'd like to connect TMDXSK437X and MCU on other EVM via USB.
Other EVM has USB2.0 type-A connect.
TMDXSK437X has USB2.0 type-A and microAB connector.
Which connect on TMDXSK437X is available to connect to other EVM…
Part Number: TMDXSK437X Hi Team,
I am using teh sitara starter kit and would like to try the USB examples
I have successfully run pdkproject create , but it did not create the usb example
How to I set it up ?
Part Number: TMDXSK437X Hi Team,
A customer is looking for a processor that can read EnDat Encoder as a Slave system. Can TMDXSK437X be use for this application?
Regards,
Danilo
Part Number: TMDXSK437X Hi Team,
I am testing boot from uart and than load application from uart and execute it
I would like to use the led blink sk demo (TI RTOS) for this test.
I am doing so on the AM437x SK, which was modified to boot from UART…
Part Number: TMDXSK437X Hi,
We are using a TMDXSK437X as our reference to build prototypes. We noticed that in many prototypes, when we try to replace either DDR or Processor, the other IC doesn't respond.
Example situation: If we have a PCBA with…
Part Number: TMDXSK437X
Hi,
Is there any particular data rate spec for the "TMDXSK437X: DDR3 Reference Design without VTT termination using AM437x" for which this design is proven for?
If yes, Can you please provide the specs or conditions at…
Part Number: TMDXSK437X
Tool/software: Code Composer Studio
we are just getting started with TMDXSK437X board and CCS.
We installed the SDK and CCS on Ubuntu 18.04
We can't locate any examples under CCS. the software displays Sitara 1.02.00.00…
Part Number: TMDXSK437X
I have a custom board with Ethernet directly connected to an on board switch (phy-less). I am trying to configure the PDK drivers to work without a phy, using a fixed configuration.The PDK I am using is for the am437x, v1.0.15…