Part Number: TMP126-Q1 Could you please share the drive strength of SIO pin of PTMP126EDCKTQ1 ( Sink/Source current)
In customer circuit there shall be a possibility to sink 5mA current by this SIO pin at 5V VDD. We would like to know whether it makes…
Part Number: TMP126-Q1 Hello Team,
For TMP126-Q1, the rise time/ fall time for SIO,SCLK, CS are mentioned as 100nS max.
Does it mean VIH level 30% - 70% or something else?
can you please clarify the test condition?
-Mahendra
Part Number: TMP126-Q1 Other Parts Discussed in Thread: TMP126 Hi there,
I had a question regarding not being able to set the Alert as expected on the tmp126. I was hoping you could have a look at my bit of arduino code and let me know if you have any…
Part Number: TMP126-Q1 Other Parts Discussed in Thread: TMP126 Hi there,
I recently added the TMP126-Q1 to a few PCBs but upon attempting to communicate with it, I'm receiving strange values.
On my first go I routed the traces to an FTDI Serial Cable…
Part Number: TMP126-Q1 Hi,
I have connected the TMP126-Q1 to my development system and am testing it. Everything is working as expected at ~room temperature. Today I put the sensor in a industrial oven to check it's operation at high temperature. The…
Part Number: TMP451-Q1 Other Parts Discussed in Thread: TMP127-Q1 , TMP126-Q1 , LM95071-Q1 , LM71-Q1 Hi, do you have such component but with SPI interface (not I2C)?
Ariel Greenbaum
Hi Kazuya,
The TMP126-Q1 is released now and you can order today.
You can view the commercial version of the TMP126 here . There is also an automotive version if AEC-Q100 is a requirement for your customers, you can find the TMP126-Q1 here . …
Part Number: TMP116 Other Parts Discussed in Thread: TMP117 , , TMP126-Q1 , TMP126 Hello,
we are in search of an accurate temperature sensor (max. +/-0.3°C accuracy, like TMP116 or TMP117) for a test and measurement project.
The power consumption…
Hi Michael,
Yes the TMP126-Q1 can be used for your intended purpose of the ALERT function. For your application, I would be sure to have the part set in Comparator Mode so that the ALERT pin is asserted once the temperature read exceeds the high temp…