Under the mcsdk_1_00_00_08 file has the project of ../evm6474l\bootloader_package\NandWriter.
when I building the project , it has the problem about
<Linking> fatal error: cannot open output file "/debug/nandWriter_debug.out" for writing
>> Compilation…
Other Parts Discussed in Thread: TMS320C6474 Hello! While developing and manufacturing the board based on DSP TMS320C6474 were made several errors in its layout:
1. Pin E7 ( RSV22 ) remained unconnected, but C6 ( RSV20 ) connected to CVdd. How far is…
Other Parts Discussed in Thread: TMS320C6474 What is the best way to interface the AM335x processor to the TMS320C6474 DSP? What would be the fastest, most efficient way to communicate between the two devices?
Charles
Other Parts Discussed in Thread: TMS320C6474 Hi,
In the following file I am exhibiting results and measurements I have carried out on a TMS320C6474
The purpose was to get a real idea of the core 0 to DDR2 write interface performance. The result I…
Other Parts Discussed in Thread: TMS320C6474
Hi,
I use a EVM TMS320C6474,
my CCS version is: 5.0.3
I setup an new target configuration and launch, when I connect target, there is a error:
IcePick_C_0: Error connecting to the target: (Error…
Other Parts Discussed in Thread: TMS320C6474 Hi All
We developed one custom board using TMS320C6474. Now we are doing board bring up, we are unable to connect JTAG Emulator to DSP(TMS320C6474) using CCS 4.1 Is it possible to find out how many TMS320C6474…
Other Parts Discussed in Thread: TMS320C6474 hi
i am having some problems in some of the TMS320C6474 which i work on and i think the source for this problems is the ddr memory ,the reason for that because i ran the code for testing the ddr which came…
Other Parts Discussed in Thread: CCSTUDIO , OMAP-L137 hello,
I am using the board for the first time. i FOLLOWED SOME BOOKS ABOUT C6XXX PROCESSORS and everytime i get errors about the memory . can somebody please tell me how to write the command file…
Hello,
I'm presently working on the same Evaluation module, i was wondering if you could help me with it. I'm actually implementing a waveform on the module and i need to know how the aif module works with edma and interrupt module. I tried to search…