Hi everyone,
I am trying to run the example codes that come with the DM6437 board.
normally when you connect the board it will run the default program which acquire video and audio data and display/play it back.
When I run the example code .…
Hi all,
I am trying connect DM6437 to the computer in via the network cable. My aim is to run the host application program as it is shown in the starter guide of the board.
I used a Dlink router and I configured the IP address of the board to be…
Hi all,
I am having a similar problem, I have connect the board and the PC via a Dlink router and I configured the IP address of the board to be static (IP: 192.168.1.100) I also set static IP for the PC (IP: 192.168.1.200) but I did not work.
I…