Part Number: TMS320DM8148 Tool/software: Linux hello,
I use 8148.
where set front porch and back porch in acquisition and separation synchronization video?
Hello,
Please could you refer the below threads:
https://e2e.ti.com/support/processors/f/791/p/432633/1628167
https://e2e.ti.com/support/legacy_forums/embedded/multimedia_software_codecs/f/356/t/365528
https://e2e.ti.com/support/processors/f/791…
Part Number: TMS320DM8148
Tool/software: Linux
Hello,
I've found some posts regardeing yocto with dm8148, but without resolution.
I thought that I can use am335x-evm as a starting point. (linux, and u-boot shall be build in standalone)
Does…
Part Number: TMS320DM8148
Tool/software: Linux
Hello,
I would like to ask if there a toolchain for windows (including gdb)
Currently we use a toolchain for linux (provided by TI), but we want to build and debug application from windows machine…
Part Number: TMS320DM8148 Other Parts Discussed in Thread: DM388 Hi all.
It is currently under development using the DM8148.
Is it correct to connect VDDQ_1V5 in DDR3 termination circuit to RDK circuit diagram?
What is VDDQ_1V5 for?
The DM388…
Part Number: TMS320DM8148 Hi
Pls. try answer my questions:
Floating address signals during boot:
I connected A13-A26 to 10K PD to set level when the address signals read at power up. Pls. advise if solve the issue.
2. Power consumption:…
Part Number: TMS320DM8148 Tool/software: Linux hi,
PIN AA6 is configured as gp1[26] via PINCNTL88 register.
PIN AA3 is configured as gp1[18] via PINCNTL87 register.
when toggling gp1[26] from 0 to 1 or from 1 to 0, gp1[26] is toggled but also gp1…
Hi, After reset mmc card starts working, not sure why, I haven't made any changes. I continue testing with resets to see if there is some issue, but meanwhile it seems stable with no errors. root@dm814x-evm:~# dmesg | grep mmc [ 0.770000] mmc0: new high…