Part Number: TMUX6219-Q1 Other Parts Discussed in Thread: TPS61046 Tool/software: Hi Experts
I am evaluating TMUX6219-Q1 and I have a few queries regarding the power of this IC.
The VDD will be connected to the output of the boost converter TPS61046…
Part Number: TMUX6219-Q1 Tool/software: Hi TI Experts,
I was looking at timing diagrams for this IC and i saw that there is a tr and tf even when they did not talk about it in the specification. May I ask for the actual rise and for time for the 15V…
Part Number: TMUX6219-Q1 Tool/software: Team,
what's the recommended EVM to evaluate this device?
I cannot find an EVM in the Q1 product folder and also not in the industrial product folder.
Best regards
Part Number: TMUX6219-Q1 Tool/software: Hi,
my customer wants to us this device with 12V VDD supply. They would like to feed a 15V signal into S1.
From my understanding, this does not work due to the following specification. Can you confirm?
Thanks…
Part Number: TMUX6219-Q1
As the picture shows, the red wine is the leakage line.
Is there such a problem, or what should be paid attention to when designing
Part Number: TMUX6219-Q1 Other Parts Discussed in Thread: TMUX6219 , TMUX7234 , TMUX4052 , TMUX7436F Hi,
In my project, I need to multiplex high voltage interfaces with 100 base ethernet and I was planning to use TMUX6219 for that purpose. S1 inputs…
Part Number: TMUX6219-Q1
e2e,
Can the TMUX6219-Q1 device handle pulses of 300mA for 1.5µs followed by 1mA for 30µs @ 15V DC? I assume, the only limitation is the thermal performance/power losses, right?
Do you have curves showing the max R_DSon…
Part Number: TS3USB221A-Q1 Other Parts Discussed in Thread: TMUX1309-Q1 , TMUX7413F , TMUX6219-Q1 , TMUX7219-Q1 Tool/software: Hi,
Can I use TS3USB221A-Q1 for CAN and Ethernet signal switching application? I see that TS3USB221A-Q1 is recommended for…
Part Number: TIDA-010239 Other Parts Discussed in Thread: TLV1811-Q1 , TMUX6219-Q1 , DRV8220 Tool/software: Hi, Team
Hope you are doing well!
My customer is bidding a small ZCU project and there is only a charging plug detection function on the board…
Part Number: SN3257-Q1 Other Parts Discussed in Thread: TMUX6219-Q1 e2e,
I'm looking for a video selector for NTSC video signals. Would you please recommend an automotive qualified multiplex to support it with the requirements below?
Requirement…