Part Number: TPD2S300 Other Parts Discussed in Thread: HD3SS3220 In the data sheet it states :-
If desiring to power the CC/PD controller during dead battery mode and if the CC/PD Controller is configured as a DRP , it is critical that the TPD2S300…
Part Number: TPD6S300 Other Parts Discussed in Thread: TPD2S300 , TPD1E05U06-Q1 , TPS65981 , HD3SS3220 When using TPD6S300 \ TPD2S300 in my USB Type C design for protection
1. Is it possible to use Vbus (4.4V - 5.25V) to supply VPWR ?
2. Should I…
Part Number: TPD2S300 Other Parts Discussed in Thread: ESD204 , TVS0500 , ESDS314 TPD2S300:
Since our spec only show 8.7V and 2.7V VM on-resistor, customers want to know the 3.45V VM’s on resistor;
What is the Surge performance? If TPD2S300 can…
Part Number: TPD2S300 I am using the TPD2S300 within in my device and the cc controller is configured as UFP.
When my device is not powered (i.e. dead battery ) and it is first connected to the Type C bus and power is provided on VBUS by the Host…
Part Number: TPD2S300 While evaluating the TPD2S300EVM and see some odd behavior that does not appear to agree with the datasheet. The cc protection does not seem to cutoff in the 100ns mentioned in the datasheet. It seems to take 20ms.
We are testing…
Part Number: TPD2S300 Other Parts Discussed in Thread: TUSB320LAI , , TPD6S300 I need to calculate the CC Line Capacitor selection.
I posted the following :-
https://e2e.ti.com/support/interface/circuit-protection/f/389/t/651056
and thus I posted…
Part Number: TPD6S300 Other Parts Discussed in Thread: TPD2S300 , HD3SS3220 DURING DEBUG - For both TPD6S300 & TPD2S300 how am I going to measure the CC capacitance to check that I have chosen the correct capacitance for the CC lines as outlined in the…
Part Number: TUSB320LAI Other Parts Discussed in Thread: TPD2S300 I need to calculate the CC Line Capacitor selection for the TPD2S300.
I posted the following :-
https://e2e.ti.com/support/interface/circuit-protection/f/389/t/651056
and thus I posted…
Part Number: TPD2S300 Other Parts Discussed in Thread: TUSB422 , TUSB320LAI , In Table 5. CC Line Capacitor Calculation it states "TUSB422 capacitance 200 450 pF From the TUSB422 Datasheet" However I am using a TUSB320LAI - what is the equivalent parameter…