Part Number: TPD4S014
Hi,
I have several questions relating to the TPD4S014 and its EVM on behalf of an engineer.
1.The TPD4S14EVM that was received upon EVM-order match the picture on the product page at TI.com. However, the EVM layout in the user…
Part Number: TPD4S014 I have got question about how to connect shield and gnd of the USB socket.
In my solution I have got two options. In first case the whole housing is made from metal and it is connected to the gnd. In second case the whole housing…
Hello
please tell me what will be the power input to shut down the output device
when I decrease the voltage from 5V down and the current is approx. 60mA
Other Parts Discussed in Thread: TPD4S014 Hi All,
I would liketo use TPD4S014 without MCU supervision. So I want to connect ACK output directly to EN input.
Is it gonna work? Please explain. See attached picture as the explanation.
Kind regards…
Other Parts Discussed in Thread: TPD4S014 Hi I have a product that uses TPD4S014 with an 10uF input capacitor. I was afraid that the capacitor might get eventually charged without a pull-down resistor but I noticed that the TPD4S014 has the voltage divider…
Jonathan,
With TPD4S014, due to the body diode of the nFET switch, if there is a short to ground on VBUS the system is expected to limit the current to VBUSOUT. Yes, a charger port can be a host, but a charger port may also be a stand alone charger…
Other Parts Discussed in Thread: TPD4S014 We have used TPD4S014 ESD protection device in one of our application in the path of USB charging circuit. IN our proto board when i connected it to Power from USB port ( connected through cable which is not having…
Other Parts Discussed in Thread: TPD4S214 , TPD4S014 I have a requirement for a USB protected switch.
My application is for a USB powered device where I must protect the device from faults occurring on USB VBUS.
I really like the TPD4S214 part because…