Other Parts Discussed in Thread: TPS2149 I'm designing in a TPS2149 but I don't plan on using it in the typical USB application. I'm going to use the switch to detect over current situations. The 3.3V LDO output will power a MCU that will monitor the…
Hello Don,
The board has two unpopulated testpoints, which should be located around the TPS2149 . Please see the picture below to locate the points on the board.
19.- EN2 signal of the TPS2149 , PWR02 signal of the TUSB2136
20.- OC signal of the…
We are using TUSB2136-TPS2149 Product Development Kit
for our project. It has built in 8052 micro controller for general purpose. We are using Keil version 4 compiler. When we compile the code we get the error message the following files are missing…
The board has two unpopulated testpoints, which should be located around the TPS2149. Please see the picture below to locate the points on the board.
19.- EN2 signal of the TPS2149, PWR02 signal of the TUSB2136
20.- OC signal of the TPS2149, OVCR1…
The following shows the procedures performed to install the kit with the TUSB2136 Computer Intel Core 2 Duo "CPU E8400 " with operating system Windows Seven 64- bit. With Windows XP the same method used below have success in installing and using the device…