Part Number: TPS23753 Other Parts Discussed in Thread: TPS23731 , TPS23751 , TPS23754 Hi,
We are using TPS23753 - PoE PD Controller in our design.
We need our design to be reviewed for the PoE PD Controller Section. I cannot share the confidential…
Other Parts Discussed in Thread: TPS23731 , TPS25750 Hello, We are planning to build an Ethernet to USB 2.0 Adapter. The Adapter shall also work as a charger getting the power via PoE+ and providing up to 20W to a device using USB Power-Delivery.
This…
Part Number: TPS2378 Other Parts Discussed in Thread: TPS2379 , TPS23731 , TPS23734 , TPS23756 , TPS23754 , TPS23754-1 , TPS23751 , TPS2373 , TPS2372 Hi Expert,
Customer looking for alternative solution for TPS2378, do you have any recommendation? …
Part Number: TPS23751 Other Parts Discussed in Thread: TPS23731EVM-095 , TPS23731 , , TPS23730 Dear Team,
Our customer new project spec as below:
8 port PD and 1 port PSE on out system.
48V convert to 5V.
System power consumption is about…
Part Number: TPS23754 Other Parts Discussed in Thread: PMP6812 , TPS23731 Hi all,
I would like to get advice about the most reasonable way to implement redundant power supply for my device by powering it via 2 DC power supplies and 1 PoE as backup.…
Hi Kevin,
Thanks for reaching out!
I would assume you plan to have 12-V 24-W isolated output power.
The following reference design boards could help:
PMP22806 (12-V 2.1A Flyback, with TPS23731): www.ti.com/.../PMP22806
PMP8812 (12-V 2.1A Flyback…
Part Number: TPS23751 Other Parts Discussed in Thread: , PMP20220 , PMP11254 , TPS23731 , TLV431 , TPS23754 Hello,
We are designing a power supply for a device with required output voltage 5V. The device will always be plugged in to a PoE connection…
Hello,
Just as a note, all IC's from all vendors will probably face a shortage. This is not unique to the TPS23758.
As you pointed out the TPS23730, TPS23734, and the TPS23731 support PSR. All of these devices are rated for higher power, so their…
Parag,
1. This is found in the EVM's of the TPS23734 and the TPS23731.
2. The TPS23731 is the cost effective solution. The TPS23734 is essentially the same IC but with an additional gate drive. If you are going to use a topology that does not need…