Other Parts Discussed in Thread: TPS2511 , TPS2543 Hi
Could you give me a test report at TPS2511?
I found a test report at TPS2543 on ESP.
1732.TPS2543 test report.pptx
Best regards,
masa
Could you double-check the mode settings v. Table 2 in the datasheet? Also, can you mention the cell phone model's checked? Remember that the cell phone must determine what it is connected to and then manage it's own current draw. The power switch current…
I see this post is from almost a year ago, but i notice the same issue. It seems there is no way to actually control SDP mode.
I expect SDP mode to be forced when the control pins are set as follows: CTL1 = CTL2 = CTL3 = 1 and ILIMSEL = 0. Instead,…
Other Parts Discussed in Thread: TPS2543 , TPS2546 We are carrying out product testing for the Lighting Global program ( www.lightingglobal.org ). As part of this testing, we will be testing USB charging ports that are integrated in off-grid solar home…
To charge the Samsung phones, you will need to use TPS2543 or TPS2546 or TPS2549Q1. TPS2543 and TPS2546 support 1.2V charging modes and you can replace the TPS2540 on the EVM with these devices (P2P compatible).
So is the answer a TPS2540 cannot support IPAD charging in the way this person has it setup? - Then how do you support IPAD charging using a TPS2543 or 2540?
Other Parts Discussed in Thread: TPS2513 , TPS2543 , TPS2546-Q1 What is our recommendations for a USB charger, to charge external device, (like mobile phone)with over load protected?
Need to protect on the 5v that will feed out ,from over load. Could…
Hi Robbie,
The TUSB320 does not support power delivery. One of these devices should work:
TPS2543
TPS2544
TPS2546
TPS65982
TPS25910
TUSB422
Best Regards,
Luis Omar Moran
High Speed Interface
SWAT Team
Hi,
TUSB320 doesn't support power delivery, you need to add a power delivery device, one of these should work:
TPS2543
TPS2544
TPS2546
TPS65982
TPS25910
Regards
Hi Jared,
The reason there's no specific device number is because it can be used a variety of VBUS switches like:
TPS2543
TPS2544
TPS2546
TPS65982 (with I2C bus)
TPS25910 (Used in our EVM)
Regards.
JC