Other Parts Discussed in Thread: TPS2543 Hi team,
The TPS2543 is rated for 3A if you use RILIM_HI = 16.9kOhm but is rated at a max continuous current of 2.5A. What would happen if I ran the part at 3A continuously? My worry is that the part may go into…
Other Parts Discussed in Thread: TPS2543 Hello.
Is TPS2543 compatible with Galaxy-Tab(Samsung)? and other Galaxy series?
If you need to get more information, please let me know.
Other Parts Discussed in Thread: TPS2544 , TPS2543 Hello,
I have some questions about TPS2544.
Please see the attached file as my questions.
7080.TPS2544 Questions.pdf
<Q1>
Could you tell me the reason why tDCHG of TPS2544 was increasedfrom…
Other Parts Discussed in Thread: TPS2543-Q1 Hello,
I have question of TPS2543-Q1
When I use TPS2543-Q1 with DCP mode, I think that the USB controller is not necessaly, is it right?
When I use TPS2543-Q1 with CDP or SDP mode, USB controller is necessaly…
Other Parts Discussed in Thread: TPS2543EVM-064 , TPS2543 Hi all,
I am trying to implement a design for a new device which has the feature to charge an IPOD but at the same time it has to offer the possibility of a USB Data connection with a PC. …
Other Parts Discussed in Thread: TPS2543 Is there a more current list of products that have been tested (charged) with the TPS2543 other than the one in ESP dated Feb 2012 ? Customer is asking if this device supports the newest Samsung, Android devices…
Other Parts Discussed in Thread: TPS2543 , TPS2546 Is it possible to connect up to 10 usb devices via 10x TPS2543 to one USB host?
One TPS2543 is in CDP mode, the other nine are in DCP mode.
All DP/DM_OUT lines are connected in parallel to the host…
Other Parts Discussed in Thread: TPS2543-Q1 I would like to confirm the operations (stop, wreck and so on) by short. I have wrote down the conditions in below.
Could you please teach them?
< Short in Pin to PIN > 1. OUT(VBUS 5V) - DM_IN 2. DM_IN …
I have a circuit with a tusb2077 that fails to release a port when a device is disconnected.
At the port, I am using a tps2543 to configure the port for phone charging. Everything works correctly except, devices will not 'unmount' when you remove them…
Other Parts Discussed in Thread: TPS2543 Dear All,
Please teach us setting of Device Control Pin of TPS2543.
When customer use DCP_Auto Mode, the setting of each CTL Pin is follows.
(CTL1,CTL2,CTL3)=(0,1,1)
(CTL1,CTL2,CTL3)=(0,0,1)
Please teach…