Other Parts Discussed in Thread: TPS2543 Hi,
what exactly is the difference between the auto detect mode from the TPS 2543 and the DCP auto detect mode from the TPS 2540/41. I can only see the different Divider Modes on the TPS2543. Could someone…
Other Parts Discussed in Thread: TPS2540 , TPS2543 TPS2540 does not use Vbus Power sw(IN & OUT pin is Open).
Can TPS2543 use only " USB charging port identification circuit "?
Vbus Power sw uses the IC which is different from TPS2540.
Other Parts Discussed in Thread: TPS2543-Q1 Hi everyone,
We at Delphi E&S, Buenos Aires, Argentina, develop radio head units which use this IC mainly as a CDP emulator and needed to know if the usual 15k pull-down resistors in the D+ and D- data lines…
Other Parts Discussed in Thread: TPS2543 , TPS2511 Hi,
Does TPS2511 not have Forced Vividre1 function such as TPS2543?
Is Divider mode of tps2511 automatically changed(Divider1 -> Divider2)?
Regards,
Kanemaru
Other Parts Discussed in Thread: TPS2543 We're laying out a board using the TPS2543 only in DCP_Auto Mode (no host) and were wondering if the DM_OUT and DP_OUT pins can be left completely disconnected or if they should be terminated in some way (e.g.…
Other Parts Discussed in Thread: TPS2543
Need to design system whose output ports have capability of providing1.5A charging current in USB-A and USB-C output ports. When both the USB port charge peripheral device simultaneously, should provide 900mA…
Part Number: TPS2549 Other Parts Discussed in Thread: TPS2546 , TPS2547 , TPS2544 , TPS2543 Hi,
Does TPS2549 have CB (IEC 62368-1) test report and certification?
Please send to me by mail.
JeffYC.Yang@arrow.com
Jeff
Thank you!
Hi David,
For TPS2557, you can't use method 2.
For TPS2543, I am not sure about that.
You can create a new thread with the device name TPS2543.
I think will related person will help reply this question.
For TI's policy, I will first click…
Hi Adam,
So what if I use TPS2543 which supports 2/2.7V and 2.7/2V divider modes. I checked with Apple's spec and these divider modes happen to match nearly perfectly with what I needed:
Divider mode
D+
D-
R1
R2
R3
R4
Max…
Part Number: TPS65987D Other Parts Discussed in Thread: TPS2543 , TPS65987 , , TUSB422 , TIDA-01620 Hello,
We have an application that's currently using a TPS2543 to enumerate a charge condition between a sinking host and a sourcing device. We're looking…