Part Number: TPS25946 Other Parts Discussed in Thread: TPS25947 Hi,
I'm doing a project where I need to protect my inputs and do some power OR-ing between two 12V sources. For that I'm using the TPS259461ARPWR which offers me the reverse current protection…
Hi Jo,
Thanks for reaching out!
We have a new device TPS25947 releasing in March and preview version is available on web. It is a good fit for USB 3.0 ,USB PD applications. It has max input voltage rating of 28V which is generally a requirement in…
Part Number: TPS2596 Other Parts Discussed in Thread: TPS25947 , Hi team,
My customer is trying to select an E-fuse which could support a nominal current of 500mA however should support an inrush current of up to 1.5A (for max 470us ). Vin is 3V3 and…
Other Parts Discussed in Thread: TPS25947 Hi, TI Support Team
There was a request for a replacement product recommendation from a customer due to the delivery issue of the following parts.
- SY6875ADBC / SILERGY
Please recommend TI products with…
Part Number: LM74202-Q1 Other Parts Discussed in Thread: TPS25980 , TPS25947 the circuit below when the input voltage drops to about 7 volts from 12 and returns to 12v the output voltage stays around 3.3V. This is not expected behavior. what can cause…
Part Number: TPS259827LEVM Other Parts Discussed in Thread: LM5069 , TPS2491 , TPS25947 Hi,
Due to high capacitive load I want to operate two TPS259827L in parallel as in the SLVA836 Application report. The application report covers the TPS259241 and…
Part Number: LM74700-Q1 Other Parts Discussed in Thread: LM74502-Q1 , , TPS25961 , TPS2521 , TPS25947 , LM74800-Q1 , TPS2663 , LM76202-Q1 Simple question - I'm considering using the LM74700QDBVRQ1 as a NMOS power (DC) switch controller. Can I connect…
Part Number: TVS1800 Other Parts Discussed in Thread: TPS25947 Hi team,
I consider using TVS1800 as transient surge protection for TPS25947 input line (absolute maximum rating <28V).
According to datasheet, TVS1800 can clamp voltage below 23.4V…
Part Number: TPS2400 Other Parts Discussed in Thread: TPS25947 hi team,
do we have overvoltage protection controller with normal voltage 20V 7A, while OVP point is 23V?
like Onsemi FPF3381 but can support 7A load current, whether FET internal or external…
Part Number: TPS25947EVM Other Parts Discussed in Thread: TPS25947 Hi Team,
My customer is surveying TPS25947 and it could be placed at customer's power board, so the thermal performance is concerned. Customer would like to know is there a TPS25977EVM…