Part Number: BQ25756 Other Parts Discussed in Thread: TPS26750 , , TPS25751 , PMP41062 In the datasheet there is a part TPS26750 mentionned to handle the CC pins. This part does not seem to exist.
I have found TPS25750D that could combine power path…
Part Number: TPS25751 Other Parts Discussed in Thread: TPS26750 , BQ25792 , BQ25756 , Tool/software: Hello, Is it possible to do Power role swaps and data role swaps with TPS25751?
Part Number: TPD4S480 Tool/software: Hi
According to the specs, VBIAS suggest a 0.1U 100V capacitor.
However, according to the reference circuit slvucp8 in the attached file, is VBIAS C50 a 0.47U 100V capacitor?
slvucp8.pdf
Part Number: BQ25750 Other Parts Discussed in Thread: TPS26750 Hi.
I'm design an EPR PD Power Source Equipment. (28V/5A)
I want to know which controller can be used in connection with the BQ2575X presented by TI EPR Solutions.
Please recommend…
Part Number: TPS25751 Other Parts Discussed in Thread: TPS25814 , , BQ25731 , TPD6S300 , TPS26750 , BQ25756 , TPS25750 Tool/software: We have an application that will charge a USBC laptop at 65W while supporting a data channel. The data source would be…
Part Number: USBCPD-APPLICATION-CUSTOMIZATION-TOOL Other Parts Discussed in Thread: TPS26750 Tool/software: When trying to import previously exported settings with EPR source PDOs in them, the EPR source PDOs get discarded, and cant be brought back manually…
Part Number: USB-PD-CHG-EVM-01 Other Parts Discussed in Thread: BQ25798 , TPS25751 , TPS25730EVM , BQ25758 , , TPS26750
Tool/software:TPS25751 、BQ25798
I prepared two batteries (single-cell 4.2V each) for a simple charging test. I’ve already switched…
Part Number: BQ25756 Other Parts Discussed in Thread: TPS26750 Tool/software: https://youtu.be/P8qNO7NDGGs
Please see above video.
I get a fault output on STAT1 & STAT2 when the voltage is under 12V, when I programmed it via hardware to have…
Hi Christopher Lim1 I've got a related basic question/ clarification that I think is appropriate to add here:
What is meant by "sink path" ?
Looking at TPS26750 ds fig 8-1 full system block diagram for example, is the "sink path" the load switch between…
Hi
I am not sure if this is the scenario of battery is missing, and i think this is not a usual user case, as the charger is always connected to Battery in the system.
if it is just a software GUI modification, I would suggest to raise a ticket to…