Part Number: TPS51388 Tool/software: Hi Team in Table 4-1. Pin Functions, FBG pin mentioned "Ground of internal analog circuitry. Decouple this pin to ground with a 4.7μF ceramic capacitor or leave the pin floating. Connect to Rfb_low if wanting to improve…
Part Number: TPS51388 Other Parts Discussed in Thread: TPS56837H Tool/software: Hello:
The current customer requires a synchronous switch buck converter that supports multiple output fast charging protocols, supports USB-C interface, PD3.1/PPS protocol…
Part Number: TPS51388 Tool/software: Hi Team,
TPS51388 datasheet only shows Vin 12V, Vout 5.15V transient response. My customer requirement is Vin 18V(typ) / Vin 22V(max), Vout 0.8V-1V, transient response <40mV.
Could you please provide transient…
Part Number: TPS51388 Tool/software: Hi All,
There is no PDF datasheet on the TPS51388 product page. Please give me a PDF datasheet.
Best Regards, Ishiwata
Part Number: TPS51388 Tool/software: Hi, I have created design using WEBENCH from link under the part page:
https://www.ti.com/product/TPS51388 , specifying Vin 11.5-16V, Vout =3.3V , Iload=3A, T=70CThen In configuration options I have chosen f switch…
Part Number: TPS51397A Other Parts Discussed in Thread: TPS51388 , TPS51397 Tool/software: Hi,
Could you please suggest a Buck switching regulator of 12 to +/-5 V which sustains up to 6A current and +/-20mV ripple
Part Number: TPS513885 Other Parts Discussed in Thread: , TPS51388EVM , TPS51388 Tool/software: this is the schematic
I’m working with the TPS513885VABR buck controller in a design that needs to support input voltages from 5V up to 24V. The circuit…
Hi Richard,
You may miss up the PN# here.
TPS513885 is the fixed output version with 5.15V output,
TPS51388 is with adj output from 0.6V-5.5V.
If the part is with 0.6V output, it should be TPS51388 then and upper FB resistor is short to vout.…
Part Number: TPS51397A Other Parts Discussed in Thread: TPS51388 Hi
The platform used by customers is Raptor Lake (Embedded)
1. Below are the two architecture diagrams of TI. Which architecture is used for i5-1345UE?
2. Please give priority to providing…