Part Number: TPS62A01A Other Parts Discussed in Thread: TPS62A01 Hi team
My customer needs the weight and reflow profile for TPS62A01 and TPS62A01A, I found the reflow profile but not the weight for the device.
Please let me know if we have weight…
Part Number: TLV62568 Other Parts Discussed in Thread: TPS62A01A , , TPS62A01
Tool/software:
Hi, I am seeking higher efficiency in 100mA to 600mA load current range at 0.9V output voltage. We are currently using TLV62568 but efficiency is too low…
Part Number: TPS62A01 Tool/software: Hi team,
Customer now are evaluating TPS62A01A now, Could you please also help to test below application usage?
Input voltage:3V
Output voltage:2.7V
Inductor: 2uH
Output capacitor:10uH
They want the efficiency…
Hi AB Singh,
Below is the normalized load regulation of TPS62A01A (FPWM) and TPS62A01 (PSM/PWM) devices For 5V input to 1.8V output.
TPS62A01A
TPS62A01
Best regards,
Varun
Part Number: DP83867IR Other Parts Discussed in Thread: TPS62A01A
Hi, We might use the DP83867IR PHY in future designs (using KSZ9031RN till now). In the datasheet I did not find any notes concerning the necessary quality (like ripple voltage) of the…
Other Parts Discussed in Thread: TPS62A01A , TPS62A01 Hi, TI expert
Customers have inquiries about DC-DC (Buck) recommendations.
Please recommend DC-DC(Buck) suitable for the requirements below.
1. DCDC Buck - Built-in OCP/Short circuit protection…
Part Number: TPS628501 Other Parts Discussed in Thread: TPS62A01A , TPS62A01 , TLV62568 Hi team,
Could you recommend a similar device with MCP1612? I choose TPS628501, I don't know if there are more suitable device, thanks.
BRs
Kian
Part Number: TLV62568A Other Parts Discussed in Thread: TPS62A01 , TPS62A01A Hello, customer needs min value for the power good threshold. We only listed typ values. For worse-case scenario he needs the min to have a defined reset for the processor. …
Part Number: TUSB8020B Other Parts Discussed in Thread: TPS62A01 , TPS62A01A , TPS62A02 , TPS62A02A , , TPS74801 Hi support team,
Is it possible to generate 1.1V VDD and 3.3V VDD33 with the following switching regulator?
TPS62A01 TPS62A01A TPS62A02…
Other Parts Discussed in Thread: TPS561201 , TPS62A02A , TPS62A01A Hi ,
We have the following design requirement in our design. Mistakenly, we have selected the TPS561201DDCR which has input voltage limitation of 4.5-V to 17-V. Now we are looking for…