The current limit of the TPS63020 is in the range of 4A (datasheet, page 5). This means it can pull more current at the input than your power supply can deliver. During startup with the load connected the input current definitely will hit that level.…
Hello Moritz,
Thank you for the response!
Please let me know the efficiency of TPS63020-Q1 for Vin 1.8-3,7V, Vout=3.3V, Iout is 0.7A.
Please let me know if you would need any other inputs
Hello EricLee
Yes, Would you please if is it possible for give me an official email so that I can send it to you.
I have another question, based on the application note "Slvaea3" which is related to the Precise Start-Up Delay can I design a circuit…
Part Number: TPS55340-Q1 Other Parts Discussed in Thread: TPS63020-Q1 , TPS55340 Hello, I wish to use the TPS55340-Q1 in sync with other supplies (TPS63020-Q1), which accepts a sync frequency of 2.4MHz +/- 200 kHz. The TP55340-Q1 would work for my application…
These kind of failure analysis (open/short tests they are sometimes called) are best done on your final system so that you can see what the impact to your particular system is. Other customers have spreadsheets where the waveform resulting from failure…
Hi,
Here is the schematic I have for the TUSB322 EVM: TUSB322 EVM Schematic.pdf
This board was made for multiple TUSB32x CC controllers so the device in the schematic (TUSB320LA) would actually be the TUSB322.
Let me know if you have any questions…
Hi Tanvi,
If I understand your requirements correctly, 3-5Vin to high current 3V LED, then the TPS63020 buck-boost converter could be used with this app note: http://www.ti.com/lit/an/slva419b/slva419b.pdf
Part Number: TPS63000-Q1 Other Parts Discussed in Thread: TPS63020-Q1 Hi Sir,
TPS63000IDRCRQ1 datasheet only show this description "Qualified for Automotive application",
We need to note the documents with AEC-Q100, Please help to provide, thanks…