Other Parts Discussed in Thread: TSC2006 , TPS65930 We use a 3.3V regulator as VBAT in our product. When the product is powered off regulator is off and there is no power on VBAT. A 3V backup battery connected to BKBAT pin H9 keeps the Real Time Clock…
Other Parts Discussed in Thread: OMAP3530 Hi All,
We are using custom board with Android Gingerbread 2.3.4 with 2.6.37 kernel version.
The suspend operation is working in following two cases.
No devices connected to OTG port
Mouse or Keyboard…
hi, Zack, i meet the same problem on TPS65930 OTG module, have you resolved it?
linux can only recongnize USB peripheral device when i first plug. and when i plug again, linux can not detect it and VBUS has not power
Other Parts Discussed in Thread: TPS65930 , TPS65920 , TPS65950 Customer observation on OMAP+TPS65930 system:
The OMAP starts correctly, i.e. the program is loaded correctly and it starts. After a random time (it may happen after a few minutes or an…
Other Parts Discussed in Thread: TPS65930 We use Omap3715 + Tps65930, wince platform, in the course of a problem is this, that after the shutdown, then the current consumption is 0mA, not sure what time, the system will go automatically restart after…
Other Parts Discussed in Thread: TPS65930 , TPA2010D1 Hi E2E community!
I am using the TI chip TPS65930 along with a small 33OHM speaker which is also utilized as a mic by simply speaking into it. I have a few questions regarding this IC that I hope…
Other Parts Discussed in Thread: TPS65930 , TPA2010D1 Hi
Now we thinking, About External Audio Speaker connect to TPS65930.
This is Audio Speaker Spec
Impedance 8 Ohm , Wattage Max 0.82W
But I I think , TPS65930 dose not including Audio AMP…
Other Parts Discussed in Thread: TVP5146 , TPS65930 Hi guys,
I have the DM370, DEVKIT8500D from Embest, and I want to connect the TVP5146.
My question is if I could connect the 1,8V from the TPS65930 to the TVP5146 supply. It is the same supply I…
Other Parts Discussed in Thread: TPS65930 We are reading an idcode of 3009002F from TPS65930A2 and 1009002F from a TPS65930B via the I2C interface. It would appears the TPS65930A2 has a new silicon version. Is that correct?
Other Parts Discussed in Thread: TPS65930 , TPS61202 Hi, We currently have the TPS65930 in our design. We are enhancing our product and some of the peripherals we need to power require 500mA. Are there any plans to enhance the TPS65930 or is there a recommended…