Other Parts Discussed in Thread: TPS65930 , DM3730 , TPS65950 , TPS65951 Hi,
We are currently working on a custom board using a TPS65930 together with a DM3730 and we would need some precision on the auxiliary audio input.
In the chip reference manual…
Hi
1.I want to have a constant output from the ADC of TPS65950 (in the main mic path) even with varying input levels.
The minimum and maximum output at any time must vary by 3 dB only.
From the data manual of TPS65950,it seems to me that if I use…
Other Parts Discussed in Thread: TPS65930
Hi all.
I am working on dm3730 with tps65930 . The board has a USB OTG port using PHY on the PMIC.Now the problem is, When I plug in a USB,the terminal Print:
VUSB3V1_DEV_GRP: 0 VUSB3V1_DEV_GRP: 40 VUSB3V1_DEV_GRP…
Other Parts Discussed in Thread: TPS65930 We are using the TPS65930 in a battery powered system. We want the device to remain off upon insertion of the main battery, so I believe we can do that using the mask on register STARTON_VBAT. We do want the system…
Hi all:
Now,I am working on dm3730 with tps65930 . I want t he board as from the device,and PC can read the board 's internal storage through the otg interface.
Anyone can help me? Thanks in advence.
Hi Guys;
We have a new board of DM3730 ,and the OTG use TPS65930 's USB ports.On DM3730 EVM board,it's use ISP1507.Now we use the DM3730 EVM BSP software to our new board.When compile the kernel ,i add the TWL4030 USB driver .After boot the system…
Other Parts Discussed in Thread: DM3730
Hi Guys;
We have a new board of DM3730 ,and the OTG use TPS65930 's USB ports.On DM3730 EVM board,it's use ISP1507.Now we use the DM3730 EVM BSP software to our new board.When compile the kernel ,i add…
Other Parts Discussed in Thread: TPS65930 , DM3730 , TPS65950 I have a device based on DM3730, TPS65930 is used as USB PHY, BSP is based on TI PSP 04.02.00.07 and there are no changes to USB stuff. It is connected to the system with USB and used as CDC…
Other Parts Discussed in Thread: TPS65930 Hello,
Could you help with the following query froma customer using the TPS65930 with an OMPA3530
We are trying to resolve an issue with running a 3.0V SDIO part on MMC2 using level shifters. The driver…