Part Number: TPS65982 Hi, Team,
Can TPS65982 disable D+/D- when TPS65982 is power on? Can we use USB RP Enable of 0x28 system configuration register? My customer would like to disable D+/D- by TPS65982 as switch when they don't use D+/D- Lane.
Best…
Hi Tim,
Depending on how you have your USB PD controller configured, it should communicate the proper data to the other device. You could also monitor the PD communication using a USB PD analyzer to confirm the data you are expecting.
The additional…
Part Number: TPS65982 Other Parts Discussed in Thread: TPS65988 , TPS65987D Hi,
it was suggested to update tps68982 based designs to either tps65987D or tps65988. Which one is preferable in which situation? Our design needs DP source and power source…
Other Parts Discussed in Thread: TPS65982-EVM , TPS65981 art Number: TPS65982-EVM
Hi
I make the TPS65982-EVM as a DRP and connected with adapters, so the TPS65982-EVM must be a sink on my test.
I saw TPS65982-EVM sent the DR_Swap and lead to unexpected…
Part Number: TPS65982 Dear all,
My customer us internal PP-5V as 5V/2A source output, I wonder how to set the over current protection point and what the accuracy of this over current.
When enter short circuit, how long will it takes to enter input…
Hi Umit,
The SWD lines are only used internally for our FW team debug. We do not recommend the customer using the SWD interface. The first time you bring up a board with the TPS65982, you should use the SPI interface and program the SPI Flash. Afterwards…
Part Number: TPS65982DMC Other Parts Discussed in Thread: TPS65982 , TPS65987 , , TPS65987DDK , TPS65988DK I want to get EVA board circuit of combination TPS65982 and TPS65987. And application note of following IC.
・ TPS65982DMC Dock Management Controller…
Part Number: TPS65982 Hi Sir,
My customer want to modify External Power Path Over-current Timeout to 81.92 ms. When we test FW v1.12.8 and earlier FW, the external Mosfet will be burned out when we test OCP funciton although we change Mosfet to 60A…
Part Number: TPS65982 Dear all,
I wonder if TI has reference code for the UCSI(Win10) derivers for TPS65982?
Or do we have any relative materials to share to help customer develop the UCSI driver?
Thanks.