Hello,
I tried this, both on J721E and J784s4, with sdk0805, and finally found it made no difference.
Here is the terminal output of my test.
MobaXterm_SerialCOM_20230208_142813.txt
Part Number: PROCESSOR-SDK-AM335X
Tool/software:
Hi Andreas Dannenberg , Liu, Frank Walzer , Anshu Madwesh ,
We are facing compilation/Build Error when we include lighttpd package in creating our own customer image.as we have lighttpd.conf which…
Part Number: TDA4VM HI Sir :
I compared the system boot time with PCIe RC enable and disable.
The PCIe will take 3.639,765 seconds.
Is there any way to reduce the PCIe initialization time?
TDA4 EVM Device Tree for Disable PCIe RC
k3-j721e…
simple_peripheral_CC26X2R1_LAUNCHXL_tirtos7_ticlang.hex.txt simple_peripheral_CC26X2R1_LAUNCHXL_tirtos7_ticlang.out.txt
OK, now I found it. The "upload" is not layouted as a button...
I had to add a ".txt" extension, otherwise it was blocked...
Part Number: TDA4VM HI Sir :
I saw RemoteProc execute for 5 seconds.
------ TDA4VM EVM
[ 10.148574] remoteproc remoteproc0: 4d80800000.dsp is available
...
[ 15.352981] remoteproc remoteproc19: b10c000.txpru is available
------
What are…
Part Number: TDA4VM
Hi TI Team,
RTOS : ti-processor-sdk-rtos-j721e-evm-08_01_00_13
Linux : ti-processor-sdk-linux-j7-evm-08_01_00_07-Linux
On the above listed SDK version on J721E based custom board, we are seeing EL1 exception on cold boots.…
Hi Nikhil,
from the logs which you shared i am not seeing any failure test case , can you let us know which test case is failing.
for a reference i am attaching the test case result at our end.
optee_j7200.txt
Regards Diwakar
Other Parts Discussed in Thread: CC2650 , BLE-STACK , CC2650STK , CC2640 Hello EveryOne.
First of all, I started the Sensortag and it works fine and connected with my phone. (Also I remember a blink led when add the battery.
Than, I started to configure…
Part Number: WL1807MOD Other Parts Discussed in Thread: AM3358
Tool/software: Linux
Hello everybody,
I'm trying to create custom Wi-Fi access point on my device, based on AM3358 and WL1807 chips. On the face of it, everything is fine: I use hostapd…