Part Number: TS5USBA224 Tool/software: Hi team,
Let me confirm the device's function when "V_AUDIO=3.3V", "VBUS=L".
1. In this situation, the audio signal coming from 6,7pin (D-/D+) reffering GND will be conducting to 3.2pin with refering GND as well…
Part Number: TS5USBA224 Tool/software:
Hi, I want to know that if I connect a 3.5mm headphones jack parallel to the TS5USBA224 with the same audio line, then it will affect the impedance across the "R" and "L" pins so much that headphones won't run…
Part Number: TS5USBA224 Other Parts Discussed in Thread: TS3USBA225 , TS3USB221 , TMUXHS221 Tool/software:
I'm trying to clarify some confusing information I've been given. Can I use a TS5USBA224 as a 2:1/1:2 mux for USB2.0 D+/D- signals? Will the shunt…
Part Number: TS5USBA224 I am working an esp32 project and want to take analog data from an FM receiver and output through a USB. I will also be using the USB for uploading data to the esp32 and charging a lipo battery. The TS5USBA224 looks like a perfect…
Part Number: TS5USBA224 Hi,
I am using TS5USBA224RSWR switch in my design as shown in below picture. The design has both differential and single ended audio signals passing through switch.
The input to input at the switch D+/R,D–/L pins comes from…
Part Number: TS5USBA224 Hi Teams,
My customer is currently surveying MAX14585/MAX14585A P2P replace solution, Can TS5USBA224 P2P replace MAX14585/MAX14585A ?
Or are they functional like solution can propose to customer?
Kai Lai
Part Number: TS5USBA224 Hi Sir,
Do you have the typical power consumption of IAUDIO? Because the maximum current is too high show in d/s(100mA), it is not easy to evaluate the product design.
We would like to know the power consumption of the following…
Part Number: TS5USBA224 I am trying to run a simulation on a circuit that uses TS5USBA224 and I need a model that will accurately represent this component. IBIS would be preferred but SPICE works as well.
Thank you!
Part Number: TS5USBA224 Other Parts Discussed in Thread: TUSB320LAI Hi team,
My customer is looking for USB and Audio switch IC like TS5USBA224 which automatically detects whether USB cable or Audio adapter is connected.
I think we can automatically…