Part Number: TUSB321 Hello,
I'm designing a USB-C audio dock. When a device (PC, smartphone, etc) is plugged in, initially the host (DFP) will provide power to the audio dock. While plugged in, ideally the audio dock should charge the host, so the power…
Part Number: TUSB321 Hello,
We have 2 problems
1. We've had some confusion on the TUSB321 VBUS_DET pin and the voltage thresholds discussed in the datasheet. In some places (ie 6.1 Absolute Maximum Ratings) VBUS_DET allows from -0.3 to 4.0V. Other…
Part Number: TUSB542 Other Parts Discussed in Thread: TUSB321 , Hello,
I have read quite a few post regarding TUSB542 and TUSB321, but still have some questions.
Schematic is attached to hopefully clarify (still work in progress).
Configuration…
Part Number: TUSB321 Hi,
Can you help us to check if TUSB321 can pass below reliability test or?
How about TUSB321AI? This one can support industry temperature range from the datasheet.
Thanks.
Hi Brian-san,
Thank you for your quick response.
Could you please tell me that reason why it isn't recommended to use TUSB321, connecting VDD to VBUS?
Best regards, Kato
Part Number: TUSB321 Dear Team,
Please review my schematic and let me know if I am missing anything.
Mode : UFP
Current : 3A,5V
Thank you!
Regards
Mit shah
Part Number: TUSB321 The datasheet states the Initialization process -
It says that after VDD is applied there is an internal POR and then the PORT pin is sampled. Can you please advise what is the delay time of the POR circuit?
Thank you,
Bara…
Part Number: TUSB321 Other Parts Discussed in Thread: BQ25616 , , TPS65987D Dear expert,
My customer need a 1s fast charger IC that support Type C standard to charge the Li-on battery. Besides 5V3A, they may also consider 9V/12V PD protocol so the current…
Part Number: TUSB321 Hi team,
We want to use TUSB321RWBR in the Device Functional Mode, and is configured to operate with 5 V power supply from the USB host side. Please tell us the status of CC1 and CC2 pins when TUSB321RWBR is not powered up.
Best…
Hi Brian,
I have compared the schematics with the reference design, no difference were found. It is also confirmed that PORT is pulled up to VDD. On the un-powered state, I checked the resistance between CC1 to GND and CC2 pin to GND when I flipped…