Hi,
We have a design for a keyboard based on TUSB3210 keyboard dev kit and generally it works fine.
However we are having a small number of failures in the field where the keyboard stops working altogether when we read back the data from the EEPROM…
Hi,
We are developing TUSB3210 Firmware using IAR 8051. The output Bin file seems to zero-padded for every 1KB. Currently the program size is 8018B and the EEPROM size is 8192B. but the zero-padding size is 178B, so the total file size is becomes…
Hi,
We are developing TUSB3210 firmware using EVM.
When performing ROM monitor debug
What RS232C cable type should be used is it straight cable or cross cable?
And what RS232C settings should we use?
Like condition of baud rate, bit, stop…
Part Number: TUSB3210 I has made a h/w board with TUSB3210 .
I want to get the source from http://www.ti.com/tool/ tusb3210kbdpdk . But I can not download it.
Can I get the source code of tusb3210kbdpdk ?
And How can I compile that code? (IAR…
Hello,
Our customers is using the CDCM6208EVM.
But they can't update the Firmware of the TUSB3210 that is installed in CDCM6208EVM. They use the PC of win7 32bit.
Is there a way to update the Firmware of TUSB3210 on a PC of WIN 7 32bit?
Best regards…
Other Parts Discussed in Thread: EV2400 Hi Team,
My customer is using EV2300 for charger and gauge programing, but it's found EV2300 and EV2400 is easy to damage.
It's found that it's actually TUSB3210 chip inside that's damaged.
Some questions…
Dear Sir
We would like to design USB to I2C dongle ,do you recommend to use TUSB3210
Or you have another suggestion ?? Have anything I need to take care when I designed ??
Thanks
Part Number: TMP007EVM Hi ,
I would like to implement the control on single TMP007 IC using matlab, in order to evaluate its performance in company existing system.
Could you please advise how to send data ( commands/text...) from host PC, via USB…
Hello, please am tried install the hardware usb interface adapter 2006 but my laptop not found the port, any have a suggestion or the driver correct? Because I used the packet sllc288,sllc160a,slvc291,sllc443a ,ev2300a and continued with the problem …