Other Parts Discussed in Thread: TMS320VC5416 , TUSB1105 , TUSB3410 Hi everyone,
I need to make USB communications for my DSP (TMS320VC5416) and want to know if the TUSB3210 is the interface to use, or just a TUSB1105 transceiver. I'm assuming with…
Hi,
Our customer is using TUSB3210 for PS2 to USB converter,
initially the PS2 lines (data and clock) were connected to the GPIO ports
Port 0(0.0 & 0.1), but there were issues like few keys on the PS2 keyboard doesn't work
properly or…
In the Keyboard firmware source code downloaded from TI there are two files kb3210.i2c and kb3210.bin under \Release\Exe.
What is the file kb3210.i2c? If I used the Apploader drivers to load kb3210.bin to the tusb3210kbd rev3 it would work .
Was…
Greetings, My name is Cristian Dolha (or just Chris), and i'm currently studying in Finland. I've been an audio DIY-ist for quite a few years now, and i've recently discovered / become interested in TI DSP chips. They, in combination with some class D…
Other Parts Discussed in Thread: TUSB2036 When I run the TI USB EEPROM Burner utility on my TUSB3210 design I get a USB Hub Power Exceeded error in windows.
My designed is set to run on bus power however when I load the EEPROM Burner firmware it wants…
can someone tell me that the IT program Tusbxxx eeprom burner gives me the error: (Eepromburnerdlg) (OnInitDialog) Registerfordevicenotification fail (Error 13) doi him to accept after the error window and opens the program but no devices appear in the…
I use TUSB3210 develop a USB to IIC bridge. I download code from PC. Now my code can receive the first setup packet (get device description).
when I respond the "get device descrition", I can only send first 8 bytes to PC only. The standary packet has…
Team
For USB designs with TI's TUSB3210, can the end product use TI's VID and PID, or is it mandatory for the developer to acquire their own Vendor ID? Please advise.
In advance, thank you for your assistance.
On my college they've build a custom board with the TUSB3210 on it. More information about it here: http://www.tusb3210.com
They use the driver apploader and eeprom burner from TI. It works
all fine under Windows XP, but now I would like to use it under…