Part Number: TUSB422 Hi Team,
Is there reference code for PPS such as QC4.0 in the power negotiation? If so, could you please share the reference code, thanks!
Best Regards!
Hao
Hi Olof,
TUSB422 does require a external MCU and cannot be configured as a "listener" in default FW. I will look into other details and get back to you next week.
Note: There is a US holiday on 11/28 & 11/29, responses will be delayed.
Hi BHautik,
Please go to the TUSB422 product page and click the "Request software" link just above the Technical Documentation section of the page. TUSB422 code is best source to answer your questions. PD messages sent to TUSB422 need to be read from…
Part Number: TUSB422 Other Parts Discussed in Thread: TUSB320 Hello,
We are using the TUSB422 in a DRP mode for power only. We are not using PD, only 5V up to 3A options.
When we plug in a Type C PD charger to our TUSB422, the devices get configured…
Part Number: TUSB422 Hello Team ,
my top assigned account is planning to use the TUSB422 for TYpe C PD negotiations in a sink only device .
Can they configure to make sure the INT_IN pin is not connected to any uC .
Due to their manufacturing capability…
Part Number: TUSB422 Hi. I got a same issue in this question. link is down below.
https://e2e.ti.com/support/interface/f/138/t/702096?jktype=e2e
and I also download this file.
USB Type-C to DP Dongle Firmware
this file have too many hexadecimal…
Part Number: TUSB422 Other Parts Discussed in Thread: MSP430FR59941 Hi,
I've been working on porting the TI code for the TUSB422 over to our MSP430. So far I can't get past the PE_SNK_WAIT_FOR_CAPS stage. I'm a sink and I have a PD sniffer hooked up…