Part Number: TUSB422 I see plenty of messages from the source, and I even see the TUSB422 respond with a GoodCRC. However I never see the RECEIVE_BYTE_COUNT register increment, even when the RX_SOP_STATUS is set. Still the "hardware" does not update the…
Part Number: TUSB422 Hi,
I want to supply my project with 20V form standard charger with USB PD. On my PCB i want to use TUSB422 as a PD controller. I would like to ask, which registers should be set to receive 20V on VBUS (when TUSB422 is configured…
Part Number: TUSB422 Hello,
we have designed a board using TUSB422 for usb-c power delivery and following your schematic.
We are using a microcontroller to run your reference firmware code, but unfortunately we are not able to go through the whole…
Part Number: TUSB422 Greetings.
My company currently manufactures a USB data collection device that talks to a Samsung tablet via its micro USB OTG port. Our device is also responsible for charging the tablet, so it behaves similar to a docking station…
The TUSB422 controller feature is integrated inside the charger. Please refer to the application note that explains this TIDA, and the Figure 1 diagram shows the TUSB422 block inside the charger.
Part Number: TUSB422 We are trying to use "PD & USB alternative mode" for display port on the LK (bootloder).
Is it possibe to make PD Stack for LK?
If it is not possible, We need to reason technically.