Part Number: TUSB422 Hi Sir,
I know TUSB422 could record VBUS voltage in register for MCU to read, but...
1. Now using TUSB422 as DFP device and provide 5V already, if UFP want to get highier VBUS like 12V, is it passible UFP could communicate with…
Other Parts Discussed in Thread: TUSB422 , MSP-EXP430FR5969
Hi Team,
We are looking for the suitable MSP430 for TCPM and found TUSB422EVM Quick Start Guide(SLLU252).
According to this user’s guide, the TUSB422EVM can operate stand-alone…
Hello,
It is possible, You only have to configure the TUSB422 and read it's status when the TCPC asserts the interrupt and configure the VBUS and Signal switches accordingly (actually that is what a TCPM does).
Regards,
Diego.
Part Number: TUSB422 Dear Community For a project we want to get 20V and 3A from an USB-PD adapter for our device consuming power of the USB port (Upstream Facing Port (UFP) mode). I discovered the TUSB422 as a very nice solution for power bigger than…
Part Number: TUSB422 I cannot, from the datasheet, seem to determine any way to have the 422 request higher voltages to be applied to vbus from a given source. Is this possible or must we manually do this using the USB type c spec?
Part Number: TUSB320LAI Other Parts Discussed in Thread: TUSB422 , , TUSB320HAI Hi Sir,
I would like to inquire whether you have a USB Type-C CC logic device that supports CC1, CC2, and VBUS detection pins with support for 25V input Voltage. Additionally…
Part Number: HD3SS3220 Other Parts Discussed in Thread: TUSB422 Tool/software: Dear teams,
1. I think HD3SS3220 includes USB 3.0 switch and PD charging, right?
If I use this one, I don't need TUSB422, right?
2. HD3SS3220, my device can be understood…
Part Number: TMUXHS4212 Other Parts Discussed in Thread: TUSB422 , TUSB322 , TUSB321 , TUSB320 Tool/software: Hi team,
The customer is considering using the TMUXHS4212, and is also evaluating a controller to pair with this MUX.
Ideally, they are looking…
Part Number: TUSB544 Other Parts Discussed in Thread: TIDA-01620 , TUSB422
Hi Team,
Posting on behalf of our customer.
I have been looking into one of your products (TUSB544) and the documents available left me somewhat confused.
The datasheet…