Part Number: TVS2200 Dear Team,
My customer is evaluating the TVS2200DRVR to clamp surge on AC Adapter input line of VIN=19.5V. They would like to know the following characteristics of surge clamp of the TVS2200.
1) Is there a characteristic diagram…
Part Number: TVS2200 Tool/software: Hi expert,
Customer would like to know if the TVS2200 GND side has layout limitation and cannot connect to the PGND plane of the surface side which means TVS2200 GND is an independent small plane. If so, then how…
Part Number: TVS2200 Hi team,
we need I-V curve to show our dynamic resistance to customer,
datasheet only have large scale.
we need a curve around same scale as below one, please support this thanks
Part Number: TVS2200 HI team,
1.can I see surge protection device as the ESD device but with very low dynamic resistance?
2.and why type-C power line recommended add a surge protection but data line normally don't?
Part Number: TVS2200 Other Parts Discussed in Thread: TVS3300 , The maximal voltage rating of flat clamp device available now is 33V (TVS3300). Can I use 2 TVS2200 in series to form a up to 44V level surge protection device?
Part Number: TPS65994AD Other Parts Discussed in Thread: TPS65994 , TVS2200 Hi,
How close should TVS2200 be placed at TPS65994/VBUS pin? Does it need to be very close? What is the side effect if it's placed close to the type-c connector instead of TPD65994…
Part Number: TVS2200 Other Parts Discussed in Thread: TPS65988 , TVS0500 Hi Sir,
As the title, customer are using the original part with Amazing Microelectronic TVS "AZ2015-01H", could we replace it instead by TVS2200?
Please help to review it and…
Part Number: TVS2200 Hi team,
As TVS2200 is a recommended solution to work with TI PD controller especially in PC market, customer would like to know how should they design the experiment to verify TVS device is working? Is there a typical test standard…