Part Number: TXB0108 Hi Experts,
We are performing a SI simulation on a board that includes the TXB0108DQSR IC. During the simulation, we are observing non-monotonic behavior in the waveform.
The issue occurs specifically when using the txb0108.ibs…
Part Number: TXB0108 Other Parts Discussed in Thread: TXS0108E , Hi Team,
We are using TXB0108DQRS part in our board. we are doing signal integrity analysis for it. here, we are observing non-monotonic behaviour in our waveform.
This issue was raised…
Part Number: TXB0108 Other Parts Discussed in Thread: TXB-EVM , TXS0108E Hi Experts,
We are performing a SI simulation on a board that includes the TXB0108DQSR IC. During the simulation, we are observing non-monotonic behavior in the waveform.
The…
Part Number: TXB0108 Other Parts Discussed in Thread: TXB0604 , TXS0108E Hi,
We have used TXB0108 bidirectional buffer in 1.8V logic (Vcca & Vccb). In the datasheet for Vcca & Vccb = 1.8V, the maximum data rate supported is 52Mbps. Our SPI clock is…
Part Number: TXB0108
Tool/software:
I have a query regarding the MPN: TXB0108 8-Bit Bidirectional Voltage-Level Translator . There appears to be a discrepancy between the Top View diagram on Page 3 and Section 4.1 on Page 5 of the datasheet, specifically…
Part Number: TXB0108TXB0108RUK datasheet does not state the pinout for this package. On one datasheet it has 6 pins on two sides and 4 on the other two sides. However it then shows the package information as 5 pins on each of the 4 sides in the WQFN…
Part Number: TXB0108 Tool/software: Hi Team,
We are using TXB0108 in our design. We have connected open drain pin in this level translator with the pullup of 2.2K. Functionality side we are not facing any issue. It is working fine. But in datasheet…
Part Number: TXB0108 Tool/software: Dears,
The customer uses a level conversion chip, and the specific application is to realize PBI bus communication between DSP F28377D and a communication board. Now I want to choose a bidirectional level conversion…
Part Number: TXB0108 Other Parts Discussed in Thread: TXU0304 , TXU0104 , TXU0204 Tool/software: Dears,
My customer use our TXB0108. The DSP signal level is 3.3V, and the MVB board signal level is 5V. TI's TXB0108pwr level conversion chip is used…