Hi Tom,
Thanks for your replies.
1. I had test one known good board(not the EVM, just another), the resistance between C6670's CVDD and VSS is around 8 Ohm. But on my board, I got the resistance value that is less than 1 Ohm with the same test equipment…
Other Parts Discussed in Thread: UCD9244 , UCD7242 Hi,
We are using UCD9244 PWM contrller with two UCD7242 power driver for generating the voltages 1V,1.2,3.3V & 1.8V . We have programmed the PWM controller and the voltages are generated and worked…
Other Parts Discussed in Thread: UCD9244 , UCD7242 , UCD9222 , UCD9224 Hello!
We use two UCD9244 + 2 x UCD7242 in our project for Zync7000 FPGA supply.
We have two problems:
1. How to program UCD9244 Power Good pin #24 by means of Fusion Digital…
Other Parts Discussed in Thread: 66AK2H14 , UCD7242 , UCD9244 Hi all,
I met a very strange phenomenon.
In my design, I used UCD9244+UCD7242 to generate 1.8V to 66AK2H14's 1.8V IO. But there are two beads between the power rail and the 1.8V IO. …
Other Parts Discussed in Thread: UCD9248 , UCD7242 , UCD9248E Hi,
I have some trouble with the input voltage to the UCD9248 with a UCD7242 driver. When I turn off the input power supply to the UCD9248, the input voltage slowly drops (due to a supercap…
Other Parts Discussed in Thread: UCD9222 , UCD7242 Dear SIR'
Does the fusion config file for C6678 be the same with C6655?
On our board, the core power controler for C6655 is UCD9222+UCD7242.
UCD9222 does not come with a default configuration, it can be used with a wide variety of applications.
The Fusion Digital Power Designer (FDPD) software is used to create the configuration for the UCD9222 controller.
There are a number of methods…
Hi Tom,
thanks for your insight! We will do some additional testing / measuring concerning CVDD/CVDD1 and AVDDA1/2/3 to rule out any voltage drops / current starvation.
In general, the design is largely based on the C6678 EVM kit, so we're using…
Other Parts Discussed in Thread: UCD9244 , UCD74120 , UCD9222 , UCD7242 , UCD7232 , CSD87353Q5D Hi TI experts,
I want to acquire higher current, so I use one UCD9244's channel to generate PWM signals to control two UCD74120 simultaneously.
Two FLT…