SI,
Please see the attached presentation. It was originally prepared for the LM10010 which was later superceded by the LM10011 which has higher precision. Please also see the many E2E posts discussing the LM10011 and TPS56121 with C667x and C665x. …
Neema
Along with the EVM, a DVD is shipped which encloses everything needed.
-
However, please find attached.
0246.K2H_K2EVM-HK_SCH_A102_Rev1_0.pdf
Regards
Shankari G
Neema
Along with the EVM, a DVD is shipped which encloses everything needed.
-
However, please find attached.
K2H_K2EVM-HK_SCH_A102_Rev1_0.pdf
Regards
Shankari G
Other Parts Discussed in Thread: UCD9244 , UCD7242 Hello,
I use the UCD9244 pwm controller to controll a power driver UCD7242.
The UCD7242 has a VIN of 5V and shall generat 3.3V on Port B.
I configured the UCD9244 to generate a 1MHz PWM with a Pulse…
Hi,
My customer want to use the BOC to connect two EVM6670 for AIF2 test. Their are two EVMs, one version is TMDSEVM6670LE Rev.3A, the other is Rev.4A. From below figure extracted from the TMDXEVM6670Lx_EVM_REV_3_0_DSN.pdf, the TIMO0 is connected to…
Part Number: TCI6638K2K Hello,
We have designed a enodeB Board based on K2K EVM design.
The query is the SPI interface of K2K interfaced to serial DAC used to control the VCXO.
The K2K SPI is 16 bits, but the DAC (DAC8550IBDGKT) is of 24bits. Is…
Hi Qian,
There are reasons for us to go with UCD74120:
[1] This regulator is an easy match with UCD9244EP for smart reflex aspects.
[2] This regulator along with UCD9222 used in EVMK2HX_ K2H_evm (schematic of the EVM is attached).
[3] In one of…
Part Number: UCD9090 Other Parts Discussed in Thread: UCD9244 , , TCI6638K2K , UCD74120 Dear Sir/Ma'am
We are working with UCD9090 and UCD9244 for power sequencing and monitoring operation. Fusion Digital Power designer is the tool used for configuring…
Other Parts Discussed in Thread: UCD9244 , UCD74120 , UCD9224 Hi all,
I used UCD9244+UCD74120 to generate 1.0V to supply the Keystone II SOC's core power.
Now we have not mounted the SOC yet. We just debug the UCD9244+UCD74120.
And I met a problem…