Hello,
Does anyone know how to find out the actual size of code when downloaded to the chip, using IAR for ARM?
The problem is that I want to see if both zstack and Wmbus stack fit in CC2538 .
Probably the do, since there is a CC2538 + CC1200 EVM…
Hi Victor,
yes, CC430 can support the WMBus protocol, which is described in the EN13757-4 (and -3, -5) documents. In fact the CC430 is the perfect single-chip device for WMBus, where you can put the entire stack on chip and even some application code…
Other Parts Discussed in Thread: WMBUS , CC1125 Hi,
for wireless mbus t mode the transmitter datarate varies from 90 to 110 kbps. I used recommended wmbus t mode settings ( http://e2e.ti.com/support/low_power_rf/f/155/t/146435.aspx ), set toc_limit…
I used the settings I posted for receive performance testing where the preamble setting does not have any effect. Hence I used default values but the correct preamble is 0x55.
The same is true for dual sync word search. I checked for basic radio performance…
Other Parts Discussed in Thread: CC1101 , CC110L Hi,
TI has a wireless m-bus app. software for CC1101: http://www.ti.com/tool/wmbus
Is it also valid for CC110L+MSP430?
Part Number: CC1200EMK-868-930 Other Parts Discussed in Thread: WMBUS , CC1200 , CC1125 , CC1310 , CC110L , CC1350 , CC1101 , LAUNCHXL-CC1310 Hi,
I would like to collect/sniff data(no transmission) with a CC1200 Evaluation Module with XTAL 40Mhz,…
Other Parts Discussed in Thread: CC1120 , WMBUS I would like to know how to fix the register settings with using SmartRF studio. In my customer's system, they would like to configure 200kbps BW. However, if only the BW is changed, RSSI becomes worse.…
The settings looks correct. Also, if you set the same settings on both sides it should not matter if the frequency was not correct.
I haven't made settings for the different channels but for N mode these could be used: processors.wiki.ti.com/.../Category…
Part Number: CC1125
Hello,
We are doing the development part of a E-meter that will work as a Collector in a Wireless M-bus communication using the CC112X transceiver. We have doubts if we are filling the time requirement in the telegrams sent from…
So,
I received from a Vector Signal Generator a WMBUS - N1g packet (4-GFSK with Preamble 0x77777777; Sync word 0xFF7D D5F7; lenght byte; data 27byte; crc )
Normal
0
14
false
false
false
IT
X…