Eddie,
We see the problem on some devices but randomly and only after a lot of reading, never after a power up. A small precision : in some cases, depending on the relative location of the tags, one antenna can "see" several tags, the main and others…
Other Parts Discussed in Thread: TRF7960 , TRF7960A Hi,
i have a problem.
I interfaced the reader TRF7960 with a mc9s08gb60 . An error occurs when the collision have been running my code but when re-run the inventory the RFID reader…
Yes, we are using the TI software "sloc297c(TRF79xx_Eval_Board_Source)". We interfaced the TRF IC with a PIC MCU over the SPI. The MCU communicates with the host over UART interface.
*****
Full Communication Chain
We get a "Get Tag ID" command…
Hi Bert,
Bert Gerrits said: At the moment I noticed a "obsolete" status by; " DRV8412DDW ". The link: DRV8412 | Buy TI Parts | TI.com Bert Gerrits said: As far as I know it is the exact same component. Could je please tell me, is the component: "active…
Hi Paul. We did not find any dropped packets of this type on the firewall.
Only these requests reached the destination server:
192.91.75.12 [07/Mar/2023:12:44:55 +0000] "POST ...inventory HTTP/1.1" 200 2 (PartNumber TESTOPN - maybe runned by save…
Hi Xia,
SN65DSI84ZXHR is a low inventory part that has a maximum order limit. It looks like you have ordered the part within the last month, and are receiving the following error on your create order requests:
"errors": [
{
"errorCode": "ERR-TICOM…
Hi Nan,
It looks like you're sending requests to two different APIs:
Product inventory and pricing API ( /v2/store/products )
Inventory subscription API ( /v2/store/subscriptions/inventory )
Only the requests to the inventory subscription…
Hi Chikku,
SLAA471 says that '550x and '5510 are not susceptible. They are immune. The other 55xx and all 54xxA parts seem to be susceptible though.
Our application just started production using the '5529. During development, we never saw this error…
Hi Zane,
If you call the pricing and inventory API, you'll find that each of these parts has an order limit, indicating that only part of the total available inventory is available to one customer for ordering, Order limits are sometimes imposed on…
Hello Jon,
The level-shifting transistor inside the HS Bulk Sense block is a PNP device, not NPN. Usually this controller is used in a "universal-line" AC input application, and PNP transistors with 400V+ ratings are relatively easy to find.
In your…