Daniel,
This is just telling you that if you have an AC coupled input, the ADC inputs are referenced internally through these resistors and you do not need to provide any type of reference. You will see this if you look at the ADS42JB69EVM schematic…
Part Number: TPS2490 Other Parts Discussed in Thread: TPS24770 , TPS24720 Hi Sir
TPS2490 will be use in 12V/14A ~160W.
Maximum continuous load current is 16A
VCC = 13 -10V
N-MOSFET : SM4373NAKP
Pls help why we key the value in excel file,…
Part Number: SN74LVC126A Tool/software: Hi team,
My customer plan to use SN74LVC126ADR in their design, they need a datasheet with footprint inside it, but the online datasheet get no footprint info available.
In my hand, I get an previous verion…
Yaron,
Try the following points for using the Auto Re-Arm Trigger.
1. The Trigger option in the HSDC Pro can be configured as “Auto Re-Arm Trigger” to capture a specified Number of Samples Per channel for each external trigger that occurs at “EXT_TRG_INPUT…
Other Parts Discussed in Thread: TX517 , AFE5809 , ADS52J90 , AFE5801EVM , AFE5801 , AFE58JD16 , AFE5816 , AFE5851 , ADS5294 , TX810
How to create an ultrasound system from TI’s ultrasound portfolio?
The signal chain would be TX517 -> transducer…
Henry,
This part will not work in single-ended mode. See the schematic attached for using a transformer input example.
Regards,
Jim
ADS42JB69EVM-SCH_D.pdf