Part Number: MSP430F5438A Other Parts Discussed in Thread: MAX232 , MSP430F5529 Hello, Texas Team or Experts
My MCU have to communicate RS232 with MSP430F5438A.
So, I found the example of uart loopback in CCS Resource Explorer and then I downloaded…
Hi Fatmawati,
Below is my connection details of MSP-FET to the target development board MSP-TS430PZ5x100:
MSP-FET Target Development Board (JTAG)
TEST TEST
RST RST
UART_TXD P1.1/ Pin 18
UART_RXD P1.2/ Pin 19
VCC_TARGET VCC_TARGET
GND…
Hi Eli, Those are the best fits I can find as well. The target boards for MSP430F2619S-HT are MSP-TS430PM64 and MSP-TS430PN80. For MSP430F5438A-EP, you can use MSP-TS430PZ5x100. Take note that these boards are not hi-temp, so do not temperature cycle…
Table 1-1 of the Hardware Tools User's Guide (SLAU278) shows that the MSP-TS430PZ5x100 supports the MSP430F543x, MSP430BT5190, and MSP430SL5438A devices which have P1.0 at pin 17. I recommend the MSP-TS430PZ100USB for MSP430F5659 devices where P1.0 is…
Hi Clemens,
This is my first time working with MSP430 so I have quite a number of queries. Sorry in advance on bombing you with so many questions.
I would like to clarify few things about the UCS operations in MSP430F5438A with respect to MSP-TS430PZ5X100…
Ok, for a little background, my situation (processor type, schematics, everything) is identical to this original question/issue, here's the link:
CCS/MSP430F5438A: Going from JTAG to Spy-Bi-Wire Troubleshooting
Also, to answer some questions:
…
Hello DJ,
Are you looking for Experiment board for MSP430F5419AIPZ (100 pin LQFP). it is pin-pin compatible with MSP430F5438A with difference in Flash so customer can use MSP-TS430PZ5X100 or MSP-EXP430F5438.
Regards,
Vikas Chola
Hello,
Go Bravos said: My customer has been using the MSP430F5438 and are wondering what exactly will happen if they do not rebuild the code using the 438A version’s header and linker files.
They’re reading the migration guide , but it is going to…
Hi Donghyeon,
Do you have a TI-built EVM to test on, like the MSP-TS430PZ5X100 or MSP-EXP430F5438, and if so then do these yield similar results? Have you also tested with LPMs, different MSP430 CPU frequencies, and core voltages? Please provide the…