Hi, I keep getting a similar error, I have tried upgrading to the newest SDK ti-processor-sdk-linux-am335x-evm-01.00.00.03
wpa_supplicant v2.1-devel
random: Trying to read entropy from /dev/random
Successfully initialized wpa_supplicant
Initializing…
Part Number: TDA4AL-Q1 I followed this document to configure mcu SPI2 and SPI4, and ran the use case and found that neither party accepted the data
SPI Enablement and Validation on TDA4 Family.pdf
Here is the log that runs
root@j721s2-evm:/home…
Part Number: TMS320C6657 Tool/software: Code Composer Studio Dear TI Support Team,
I am using the latest Processor SDK of C6657 and the CCS v7.0.0 and v6.2.0 as well. The NIMU/EMAC driver has been corrected with a lot of patches to work correctly in…
Hello Marc,
I am bit confused. Does SDK support 7" LCD that come with the EVM package? What type of interface is used for the connecting LCD (available with the EVM package) to the processor?
In our design we will use indepedent resistive touch…
Other Parts Discussed in Thread: AM3505 Hi,
I have question about MMC/SD card license, btw the processor is AM3505.
1)Will the certification of SD Association be necessary when the product(processor is AM3505) works as SD host ? And do we need to…
Chris,
Can you please provide more details about how your system is partitioned between host and DSP? I assume that data I/O etc happens on host processor and you feed the raw data (over PCIe) for DSP processing.
Desktop Linux SDK contains the foundational…
i am using a AM335x Starter Kit from Sirtex. output of cpuinfo Processor : ARMv7 Processor rev 2 (v7l) BogoMIPS : 718.02 Features : swp half thumb fastmult vfp edsp thumbee neon vfpv3 tls CPU implementer : 0x41 CPU architecture: 7 CPU variant : 0x3 CPU…
Other Parts Discussed in Thread: AM3358 Hello!
I just found myself writing this code in my .CFG file:
var SPIPkg = xdc.loadPackage('ti.drv.spi');
in order to link with the Processor SDK for TI-RTOS's (v3.0) SPI library. However, I see that some…
Part Number: AM5726
Dear All,
we have a monochrome image sensor connected to an FPGA which converts the pixel data from serial to parallel. The pixel data is then transferred to VIN1A of an AM5726.
The pixels are not read out and transferred in…
Part Number: AM62A7 Other Parts Discussed in Thread: TDA4VH-Q1 Tool/software: Hi,
Yocto SDK: 09.01.00
EVM: AM62A
We are using AM62A7 processor and camera sensor attached to it. We are using below pipeline for streaming.
gst-launch-1.0 -e v4l2src…