Thank you for your answer,
I improved the tapering of current, and now I can get the FC flag set, and correct values for VOK. But following the learning procedure, in my log the Learned status goes from 4 to 6 (skip the 5 value). And the Max Error goes…
Hi Sammi,
Thank you for your support. Can you try these files?
2821.[log] ChenID=1297, Charge Volt=3950mV, Term Volt=3500mV(After learning).xlsx
[gg file] ChenID=1297, Charge Volt=3950mV, Term Volt=3500mV.zip
[srec] ChenID=1297, Charge Volt=3950mV…
Other Parts Discussed in Thread: PTH08T250W Gentlemen,
I have three questions on the PTH08T250W.
I would like to put three in parallel and cannot find that this is ok. All examples are only for two in parallel and there is never any mention that more…
Part Number: MSP430F5528 Other Parts Discussed in Thread: TMP1075EVM , TMP116 , TMP1075 Tool/software: Code Composer Studio NEED SOURCE CODE FOR MSP430F5528 USED ON TMP1075EVM
ANY HELP IS MUCH APPRECIATED.
THANKS!
Part Number: CC3200 Hi everyone , i want to ask you some questions:
-can I feed with another power source the Sensortag Simplelink cc3200 that is not the AAA Bateries ?.
-If the Sensortag Simplelink cc3200 turn off , do I have to install the filmware…
Part Number: BQ34Z100-G1
We are currently using the BQ34Z100-G1 in the battery packs for our device. We have noticed the estimated time until empty is very inaccurate at low loads (100-200mA). We have also noticed the fuel gauge estimated minutes until…
Dear Onyx san,
When the log acquisition method was changed, RUP_DIS was cleared and the learning cycle was completed (QMAXUP = L⇒H, RESUP = L⇒H).
NG:Watch(Interval=2000ms), All Registers, All State Parameters, All Registers Parameters, Total 49 items…
Part Number: BQ40Z50-R1 Other Parts Discussed in Thread: GPCRB
HI, TI team
I used the bq40z50r1 in the project. The pack is discharged under about 7degC. However the RSOC have sharp knee from 10%, not decreased gradually. How could i to optimize the…
See from row 6660 in PACK_132 for the transition to 0 RSOC (highlighted yellow)
and row 6424 in PACK_124.
Pack_124_100-0_RSOC.xlsx Pack_132_100-0_RSOC.xlsx
Hello.We are going to do a project on sleep monitoring device using voice assistant model.We have been searching here and there for the sensor which has to be used for sleep monitoring.It will be your most kindness if u guide us in this regard.
please…