Part Number: BQ27542EVM Tool/software: Dear TI support team,
I am using the BQ27542 for a discharge test and found that the SOH suddenly drops.
Why did the SOH suddenly drop from 100 to 97 and then further decrease to 93? After starting charging…
Part Number: BQ34Z100 Tool/software: Hi
The battery pack is in good condition before shipment; After returning, it was found that FullChargeCapacity had been updated to 0mah, and RA had also been updated abnormally; The attachment contains the log and…
Hi,
While booting my SD-Card in am335x system it suck at the below :
--------------------------------------------------------------------------------------
U-Boot 2013.10-00189-g78d8ebd-dirty (May 05 2015 - 11:18:21)
I2C: ready DRAM: 512 MiB…
Hi Batt,
this is a discharge log. I had to suspend the discharge for some time at around 4828s and continued later. The log entries during the break are deleted, but you can still see the voltage relax peak. The config for this log is almost the same…
Part Number: CC2564 We are streaming audio to a headset using the CC2564 and are noticing A3DP Overflow issues (using the TI Logger with the CC2564 TX DEBUG pin) when the headset is far away or we receive RF interference outside. We are wondering if we…
Dear Angelo,
Sorry for the late reply. We have run some test with RD and collect some data for your reference.
First , original setting, charging current 3.2A :
As you can see the setting and measure result , there are 15% off form the charging…
Other Parts Discussed in Thread: INSTASPIN-BLDC Hi,
hi, I'm using the driver drv8432 to drive a stepper motor with features that are listed in the photo. The wiring diagram I'm using is what is recommended in the demo board. For safety, I will also…
Part Number: TDC1000-TDC7200EVM Hello! I am using the TDC1000-TDC7200EVM for milk concentration analysis using the piezoelectric transducer(1 MHz) provided with the evaluation module. The goal is to calculate the FAT%, SNF%, Water Added% and density of…
Hi Biser,
Thanks for your response.
The timings are ok, i am using DDR2 (kept 256MB+256MB = 512MB) in our design. When the EVM kit comes, it shows 512MB, after that i am not seeing any 512MB using pre-built images under psp 5,6.
when i tried to…