Part Number: TPS61372 Other Parts Discussed in Thread: TPS612592 , TPS61033 Tool/software: Dear team,
My customer Lenovo is evaluating TPS61372, and they have a few questions, could you please have look?
Thank you.
1) Does the red number in…
Bad communication is a common problem engineers face with their analog-to-digital converters (ADCs). While this isn’t strictly a data converter issue, it does come up regularly and can be hard to debug. In this post I’ll talk about how to debug digital…
Hi,
Attached is a LaunchPad user's guide for a discontinued TI Cortex-M3 MCU that uses FT2232 as a USB to JTAG bridge. You will need to consider the additional cost adder using FTDI chips vs TM4C123 because I believe FTDI chips are not cheap considering…
Bardia,
Actually, there is an issue with the version on the web. We are fixing it. In the meantime, please have a look at the attached PDF.
SWRS160D_BT_HCI_Module_DM.pdf
~Miguel
S6 to BP or UART? You can verify GPIOs are on Site 2 with DMM ring out too MCU pins. Check hal.c GPIO assigned for the DRV user LED and DRV fault pin has input defined top of setupPWMs() XBAR. JP8 to J5 provide +3v3 to Lauch pad via DRV and +5v J7(on…
Hi Rakesh,
Attached eFuse part of schematic as well as design calculator sheet.
Vin = 12.00V (Clean, no ripple etc)
Vout = 0.00V (Due to enable not working)
Gate = 0.00V (as above)
Input current nom. 0.3A (this is the idle circuit current of…
Hi, Animesh,
From MX25 I found IDs as the attachment, the manufactured ID =0XC2, for device ID, I tried 0X2016 or 0X0015, for enable type, I tried 0/1/2/3. totally tried 8 cobination. All failed with the same error as the attachment.
I also attached…
Part Number: BQ28Z610 Other Parts Discussed in Thread: GPCCHEM , Hello,
We have been trying to complete a learning cycle using the BQ28Z610 EVM and a 2S1P LiFePO4 battery pack (8000mAh). We have followed the instructions in slua777 to the letter, however…
Part Number: BQ27520-G4 Hello,
I was able to successfully generate a Chem ID and updated Ra tables for our BQ27520 using this TI app note . Unfortunately we have noticed a few discrepancies in our readings -
1. State of Charge:
With a fully…
Hi Rakesh
I'm sorry to have to reply late.
Please check attached Design calculator file.
This Project is SSD Test board.
Customer doesn't want to use the OVP, UVP feature.
If the OVP, UVP feature is disabled, request the reference design.
…