Part Number: DM388 Tool/software: Code Composer Studio hello sir,
when i run the board with prepare sd card it gives me " TimeOut from Boot_proc error"
this is my log file
can you help me to solve this problem i try all possible ways but issue was…
Flash_Test.map.txt The map file shows that memory has been allocated for each array and none is marked "uninitialized".
I have attached the map file.
Regards,
Paul
Hi everyone :)
I'm new in DSP Programming world. So plz be forgiving..
I'm tring to run this project on my machine but i allways get this errors: PROBLEMS :
Description Resource Path Location Type <a href="file:/C:/ti/ccsv5/tools/compiler/dmed/HTML…
Other Parts Discussed in Thread: DM3730 Hi, I am trying to get display on DVI interface in OMAP3EVM Mistral Board with DM3730 processor module by running linux-3.7 kernel image. But I am not able to get display on DVI interface. Does linux-3.7 have DVI…
hi,Chad
I put my map file here,please take a look.
thanks
my map file for core0 is as follow:
****************************************************************************** TMS320C6x Linker PC v7.3.1 ******************************************…
Hi Jack,
The power level of 10.8W is too high for the LM5180. The LM25183 is more suitable. Take a look at this design example (+/-15V at 0.3A): https://www.ti.com/lit/ds/symlink/lm25183-q1.pdf#page=25
Here is the completed quickstart calculator…
Part Number: TPS25990
Hi Team,
We are facing a startup issue in our TPS25990-based design.
Instead of 12V in the E-Fuse output, we are getting only 2V.
We have probed the waveforms. Attached are the waveforms, schematics, and TI E-Fuse calculation…
Hello All, I am currently working under USB Camera interfacing, So i have am335x_sk with android ICS 4.0.3 and the Camera Model is of webcam pro 9000 . When i used to connect the webcam it seems to be attached in /dev/input/event2 .But the TI ICS Porting…
Part Number: CC1352P
Hi,
I have two C C1352R(Sensors) and CC1352P (collector) boards communicating with each others using sub GHz at 868 freq band, 50 KBPS speed with 12 dBm tx power with Nonbeacon mode.
We are using only by default channel mask…
HttpCore.c
//*****************************************************************************
// Copyright (C) 2014 Texas Instruments Incorporated
//
// All rights reserved. Property of Texas Instruments Incorporated.
// Restricted rights to use,…