Part Number: TIDA-01243 Other Parts Discussed in Thread: TPS65982 Hi team,
I think following link is configuration file for TPS65986 on this EVM.
And if so, are there configuration file for TPS65982on this EVM?
Best regards,
Takuya
Part Number: TIDA-01243
My customer has the following question regarding the TIDA-01243:
The Documentation says to use a dell adapter.
Page 27 , section 4.4 of the users guide: TIDUC52 .pdf
I need to know which adaptor. Also, not sure if I need…
Part Number: TPS65982 Other Parts Discussed in Thread: TIDA-01243 , , TUSB8041 , TPS65987D My customer is using the TIDA-01243 as a starting point and is adding an additional HDMI port as well as replacing the NRND TPS65986 with the TPS65982.
Here are…
Part Number: TIDA-01243 Other Parts Discussed in Thread: USB-CTM-MINIDK-EVM , HD3SS460 , TIDA-01234 , TPS65981 Hello,
I would use the USB-CTM- MINIDK-EVM ( TIDA-01243 ) to connect az USB3.0 device (4K webcam) to laptop via USB-C.
Connecting the device…
Part Number: TIDA-01243 Other Parts Discussed in Thread: TPS65982 We are looking for a solution to combine USB, HDMI and 12V power over USB Type C. We currently have a motherboard that outputs USB and HDMI which we connect to a touchscreen display. We…
Part Number: TIDA-01243 Hi,
Customer of mine wants to refer to TIDA-01243 for USB charging project.
Can I check with you if TI have the CAD files in Altium Designer version Thank you!
Part Number: TIDA-01243 Other Parts Discussed in Thread: TUSB3410 , I WANT TO USE TPS 6598X HOSTINTERFACE AND CONFIGURERATION TOOL
Can Aardvark 8PIN allow register control with GUI? without TUSB3410
p BLOCK DIAGRAM.pptx lease also check the block…
Part Number: TIDA-01243
Hi, we are using TIDA-01243 board as reference board and we want to get video out of USB-C interface. We are using MacBook Pro 2016, 15" + Samsung 4K LCD (U24E590), that is connected to USB-C.
We found, that we can get video…
Part Number: TIDA-01243 Other Parts Discussed in Thread: HD3SS460 , TPS65982 , TUSB3410 Dear Team,
My customer would like to use this TI design for dock reference.
Please help to answer below questions.
1, Is there any power sequence requirement…