Part Number: CC2652R Hi support, I am using a CC2652R board with the zc_cie example, but I need make some changes in the code and when I installed it in the board I lost pairing between the zigbee sensor and the TI board. what should I do to keep the…
Part Number: IWR6843ISK-ODS Hello,
We are looking for advice on developing a Sensor-to-Cloud gateway solution for the IWR6843ISK-ODS for multiparameter patient monitoring in a nursing home. MCU architecture and any other additional information and best…
Part Number: CC2530 The AddressSanitizer mentionned in the original question is not the only cause for exit code 1.
There are several other places (10-20) in the NWKMGR code where this happens.
Part Number: BOOST-DAC8568 Other Parts Discussed in Thread: DAC8568 Hello,
I am having some difficulty with my BOOST DAC8568 and interfacing with my Raspberry Pi. The short story is that I am able to illuminate the LEDs on the BOOST package, just not…
Part Number: DS90UB960-Q1 Other Parts Discussed in Thread: DS90UB953-Q1 Tool/software: Hello,
Could you please help me understand how to stream 4 cameras through DS90UB960 (FPD-Link III) and display them using v3link on Raspberry Pi 5 (or 4) or Rockchip…
Has anyone recommendations for a Python driver to interface a Raspberry Pi to CC110x or CC112x EVM's?
I am needing a instrumentation solution between dragging laptops into the field and custom microcontroller PCBs.
Also looking for an adapter/daughter…
Part Number: DLPDLCR230NPEVM The DLPDLCR230NPEVM says "Raspberry Pi 4 compatible out of the box," but doesn't mention Pi 5.
Has anyone gotten it working on a Pi 5?
I know Pi 5 moved DPI video output to their new RP1 chip instead of the main chip,…
Other Parts Discussed in Thread: CC2650 , CC2531 , Z-STACK Hello,
I want to implement the temperature sensor example of Z-stack home automation profile using SmartRF06 EB and CC2650. End device will be CC2650. I want to use Digi Xbee Pro series 1 dongle…
Hi YK, I have the Zigbee Linux Gateway reliably operating on Ubuntu 18.04 64-bit using the following steps: 1. Clone and install github.com/.../protobuf using the instruction provided, make sure to configure the install location ($ ./configure --prefix…
Part Number: TIDEP0084
Hello
I think I have all the credentials OK (tried several times) but keep getting same error when connecting to IBM Watson :
IBM Cloud Adapter error: Error: Connection refused: Not authorized
I have no idea what is happening…