This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

C5545 Booster Pack Demo Pgm Compiler error

i start Compile C5545 Booster Pack Sample Pgm  C55 Audio Demo

i Got the Error like below  any other tools installation required

**** Build of configuration Debug for project TIesrEngineC55 ****

"C:\\ti\\ccsv6\\utils\\bin\\gmake" -k all
'Building file: C:/ti/c55_lp/c5545bp_software_01.01.00.00/source_code/c5545bp_audio_demo/C55/TIesrEngine/src/load.c'
'Invoking: C5500 Compiler'
"C:/ti/ccsv6/tools/compiler/c5500_4.4.1/bin/cl55" -vcpu:3.3 --memory_model=huge -g --include_path="C:/ti/ccsv6/tools/compiler/c5500_4.4.1/include" --include_path="C:/ti/c55_lp/c55_csl_3.06/inc" --include_path="C:/ti/c55_lp/c5545bp_software_01.01.00.00/source_code/c5545bp_audio_demo/C55/TIesrEngine/src" --include_path="C:/ti/bios_5_42_01_09/packages/ti/bios/include" --define=C55x --define=NO_FILE_IO --define=C55x_8KHZ --define=OWN_LOAD_FUNCTIONS --define=DSPBIOS_BUILD --diag_warning=225 --gen_func_subsections=on --ptrdiff_size=32 --asm_listing --preproc_with_compile --preproc_dependency="load.d" "C:/ti/c55_lp/c5545bp_software_01.01.00.00/source_code/c5545bp_audio_demo/C55/TIesrEngine/src/load.c"

>> Compilation failure
subdir_rules.mk:49: recipe for target 'load.obj' failed
"C:/ti/c55_lp/c5545bp_software_01.01.00.00/source_code/c5545bp_audio_demo/C55/TIesrEngine/src/load.c", line 37: fatal error: could not open source file "std.h"
1 fatal error detected in the compilation of "C:/ti/c55_lp/c5545bp_software_01.01.00.00/source_code/c5545bp_audio_demo/C55/TIesrEngine/src/load.c".
Compilation terminated.
gmake: *** [load.obj] Error 1
'Building file: C:/ti/c55_lp/c5545bp_software_01.01.00.00/source_code/c5545bp_audio_demo/C55/TIesrEngine/src/rapidsearch.c'
'Invoking: C5500 Compiler'
"C:/ti/ccsv6/tools/compiler/c5500_4.4.1/bin/cl55" -vcpu:3.3 --memory_model=huge -g --include_path="C:/ti/ccsv6/tools/compiler/c5500_4.4.1/include" --include_path="C:/ti/c55_lp/c55_csl_3.06/inc" --include_path="C:/ti/c55_lp/c5545bp_software_01.01.00.00/source_code/c5545bp_audio_demo/C55/TIesrEngine/src" --include_path="C:/ti/bios_5_42_01_09/packages/ti/bios/include" --define=C55x --define=NO_FILE_IO --define=C55x_8KHZ --define=OWN_LOAD_FUNCTIONS --define=DSPBIOS_BUILD --diag_warning=225 --gen_func_subsections=on --ptrdiff_size=32 --asm_listing --preproc_with_compile --preproc_dependency="rapidsearch.d" "C:/ti/c55_lp/c5545bp_software_01.01.00.00/source_code/c5545bp_audio_demo/C55/TIesrEngine/src/rapidsearch.c"

>> Compilation failure
subdir_rules.mk:98: recipe for target 'rapidsearch.obj' failed
"C:/ti/c55_lp/c5545bp_software_01.01.00.00/source_code/c5545bp_audio_demo/C55/TIesrEngine/src/rapidsearch.c", line 29: fatal error: could not open source file "std.h"
1 fatal error detected in the compilation of "C:/ti/c55_lp/c5545bp_software_01.01.00.00/source_code/c5545bp_audio_demo/C55/TIesrEngine/src/rapidsearch.c".
Compilation terminated.
'Building file: C:/ti/c55_lp/c5545bp_software_01.01.00.00/source_code/c5545bp_audio_demo/C55/TIesrEngine/src/siinit.c'
'Invoking: C5500 Compiler'
"C:/ti/ccsv6/tools/compiler/c5500_4.4.1/bin/cl55" -vcpu:3.3 --memory_model=huge -g --include_path="C:/ti/ccsv6/tools/compiler/c5500_4.4.1/include" --include_path="C:/ti/c55_lp/c55_csl_3.06/inc" --include_path="C:/ti/c55_lp/c5545bp_software_01.01.00.00/source_code/c5545bp_audio_demo/C55/TIesrEngine/src" --include_path="C:/ti/bios_5_42_01_09/packages/ti/bios/include" --define=C55x --define=NO_FILE_IO --define=C55x_8KHZ --define=OWN_LOAD_FUNCTIONS --define=DSPBIOS_BUILD --diag_warning=225 --gen_func_subsections=on --ptrdiff_size=32 --asm_listing --preproc_with_compile --preproc_dependency="siinit.d" "C:/ti/c55_lp/c5545bp_software_01.01.00.00/source_code/c5545bp_audio_demo/C55/TIesrEngine/src/siinit.c"

>> Compilation failure
subdir_rules.mk:119: recipe for target 'siinit.obj' failed
gmake: *** [rapidsearch.obj] Error 1
"C:/ti/c55_lp/c5545bp_software_01.01.00.00/source_code/c5545bp_audio_demo/C55/TIesrEngine/src/siinit.c", line 33: fatal error: could not open source file "std.h"
1 fatal error detected in the compilation of "C:/ti/c55_lp/c5545bp_software_01.01.00.00/source_code/c5545bp_audio_demo/C55/TIesrEngine/src/siinit.c".
Compilation terminated.
gmake: *** [siinit.obj] Error 1
gmake: Target 'all' not remade because of errors.

**** Build Finished ****

  • i try to compile C5545 Booster Source Code Example. I Got the Error as Follows

    Buildfile generation error occurred..
    This project was created for a device not currently supported: TMS320C55XX.TMS320C5545.

    My Tool chain version as follows

    C5500 Compiler Tools 4.4.1 com.ti.cgt.C5500.4.4.win32.feature.group Texas Instruments
    Code Composer Studio IDE C5500 Components 6.1.0.201502111100 com.ti.ccstudio.c5500.feature.group Texas Instruments
    C55xx Device Support 1.1.4 com.ti.ccstudio.c55xx.devicesupport.win32.feature.group Texas Instruments
    TMS320C55XXCSL-LOWPWR-03.06.00.01

    My OS Windows 8.1 64 bit and Windows 7 sp1 32 bit  both not working .

    Any Help

  • i am Using CCS 6.2

    When Compile Sample Code for C5545 Booster Pack i got the Error as Follows, its release Code how the Error Come From

    where can i change it to remove the error?

    >> Compilation failure
    common/subdir_rules.mk:21: recipe for target 'common/system_init.obj' failed
    "C:/ti/c55_lp/c5545bp_software_01.01.00.00/source_code/c55xx_diagnostics/board/diag/common/system_init.c", line 65: error #137: struct "<unnamed>" has no field "CGCR1"
    "C:/ti/c55_lp/c5545bp_software_01.01.00.00/source_code/c55xx_diagnostics/board/diag/common/system_init.c", line 65: error #137: struct "<unnamed>" has no field "CGCR1"
    "C:/ti/c55_lp/c5545bp_software_01.01.00.00/source_code/c55xx_diagnostics/board/diag/common/system_init.c", line 67: error #137: struct "<unnamed>" has no field "CGCR1"
    "C:/ti/c55_lp/c5545bp_software_01.01.00.00/source_code/c55xx_diagnostics/board/diag/common/system_init.c", line 68: error #137: struct "<unnamed>" has no field "CGCR2"
    "C:/ti/c55_lp/c5545bp_software_01.01.00.00/source_code/c55xx_diagnostics/board/diag/common/system_init.c", line 69: error #137: struct "<unnamed>" has no field "CGCR3"
    "C:/ti/c55_lp/c5545bp_software_01.01.00.00/source_code/c55xx_diagnostics/board/diag/common/system_init.c", line 70: error #137: struct "<unnamed>" has no field "CGCR4"
    6 errors detected in the compilation of "C:/ti/c55_lp/c5545bp_software_01.01.00.00/source_code/c55xx_diagnostics/board/diag/common/system_init.c".
    'Building file: C:/ti/c55_lp/c5545bp_software_01.01.00.00/source_code/c55xx_diagnostics/board/diag/framework/boostC5545/src/diag_config.c'
    'Invoking: C5500 Compiler'
    "C:/ti/ccsv6/tools/compiler/c5500_4.4.1/bin/cl55" -v5515 --memory_model=large -g --include_path="C:/ti/ccsv6/tools/compiler/c5500_4.4.1/include" --include_path="C:/ti/c55_lp/c5545bp_software_01.01.00.00/source_code/c55xx_diagnostics/board/diag/i2c_dsp_msp_test/dsp_master_msp_slave/inc" --include_path="C:/ti/c55_lp/c5545bp_software_01.01.00.00/source_code/c55xx_diagnostics/board/diag/i2c_dsp_msp_test/dsp_slave_msp_master/inc" --include_path="C:/ti/c55_lp/c5545bp_software_01.01.00.00/source_code/c55xx_diagnostics/board/diag/rtc_test/inc" --

  • Senthil,

    I noticed that you have a couple other threads on this topic.

    Can I please consolidate into 1 thread? It will be easier to track.

    https://e2e.ti.com/support/dsp/c5000/f/109/t/560641

    https://e2e.ti.com/support/dsp/c5000/f/109/t/560576 

    Lali