Part Number: AM5728
Other Parts Discussed in Thread: AM5718,
Hi,
- Under each OPP level there is a max freq. for each domain, then is there a min freq. under each OPP level?
- In comparing with AM572x thermal consideration (SPRAC53–December 2016 ) and AM571x thermal consideration (SPRACI0–October 2018 ), it turns out that AM5728 in single core has lower power consumption but higher junction temperature than AM5718. Could you explain the reason behind?
for example, both Dhrystone, OPP_NOM, 25degC ambient, junction temperature AM5728(single core) vs AM5718:
58degC vs 37.4degC, delta: +20.6degC
power consumpiton:
2092mW vs 2987mW, delta: -895mW
3. In another document AM572x power consumption summary(SPRAC79–March 2017) and AM571x power consumption summary(SPRAC78–March 2017), the power consumption result are quite different from the measurements in the report SPRAC53–December 2016 and SPRACI0–October 2018.
For example, on AM5718
under same test condition: idle(MPU @HIGH, GPU @HIGH, DSP@HIGH, IVA@HIGH), 25degC ambient, the SPRACI0–October 2018 measurement vs SPRAC78–March 2017 measurement:
2295mW vs 1307mW
under minor different test condition: Dhrystone, (MPU@HIGH, MPU @HIGH, GPU @HIGH, DSP@HIGH, IVA@HIGH) in SPRACI0–October 2018 vs Dhrysone, (MPU@HIGH, GPU @NOM, DSP@NOM IVA@NOM) in SPRAC78–March 2017
4092mW vs 2956mW
It looks to me that the result in SPRAC78–March 2017 and SPRAC79–March 2017 more make sense, while in SPRAC53–December 2016 the AM5728 result is lower than expected, in SPRACI0–October 2018 the AM5718 result is much higher than expected.
Please help to clarify which document best reflect the power consumption of AM5728 and AM5718?